Hi,
This is a related question to the original thread.
The customer wants to cross compile Qt simple browser on SDK version 08.02.00.24.
He tried below steps.
1) Download Qt source code from
https://download.qt.io/archive/qt/5.14/5.14.2/qt-opensource-linux-x64-5.14.2.run
Then install
- chmod 777 qt-opensource-linux-x64-5.14.2.run
- ./qt-opensource-linux-x64-5.14.2.run
Qt tools and source codes were under /home/xxx/Qt5.14.2
2) Refer "Hand on with Qt" and setup qmake.
https://software-dl.ti.com/processor-sdk-linux-rt/esd/AM437X/08_02_00_24/exports/docs/linux/Examples_and_Demos_Sub-system_Demos.html#hands-on-with-qt
- echo $QMAKESPEC
- source /home/xxx/ti-processor-sdk-linux-rt-am437x-evm-08.02.00.24/linux-devkit/environment-setup
- echo $QMAKESPEC
confirmed QMAKESPEC was correctly configured as below
/home/xxx/ti-processor-sdk-linux-rt-am437x-evm-08.02.00.24/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi/usr/lib//mkspecs/linux-oe-g++
3) Compile Qt soruce code simplebrowser.
- cd /home/xxx/Qt5.14.2/Examples/Qt-5.14.2/webenginewidgets/simplebrowser
- qmake simplebrowser.pro
below error was show.
”Project ERROR: Unknown module(s) in QT: webenginewidgets"
Why the error is generated? Do we have any solution?
Thanks and regards,
Koichiro Tashiro