Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: TIDA-01568
I am having huge trouble bringing up a new custom target board. I have been struggeling with MLO and u-boot, but they are now running. Using SDK 8.02.
My target does not have RTC so access to RTC registers had to be removed (using defines and dts). Any access to RTC register when not running causing abort interrupt.
I am expecting that the kernel has similar problems but I am unable to find a solution or to verify that this is the case.
U-boot will run until "Starting kernel ..."
Before the above it also seems to correctly have read the kernel tracing 49xxxxx bytes read (matching kernel zImage size).
No messages after "Starting kernel ..."
I have attached JTAG with Code Composer Studio and placed breakpoints at 0x82000000 that was hit, and 0x8010000 that is also hit.
It continues to code at 0xC0F002E0 (that seems to be __mmap_switched). After a few instructions it crashes.
Apart from the RTC not being used we do not have a TPS chip for power supply. Could also be this but I would expect kernel to output something if this was the case.
I have not been able to load kernel with symbols, so I have been using Disassembly and the map file to figure out where it is.
Can anyone give a hint to how I can proceed or any help or clue to what can be causing this?