Other Parts Discussed in Thread: TPS65218D0, AM3358,
Hi,
We have a custom board with AM4378 processor and a TPS65218D0 as our PMIC. In a previous design with AM3358 processor, we had tied the DCDC2 FB line to the VDD_MPU_MON pin of the processor and it worked fine, all the rails of PMIC were producing correct voltages.
However with our new design with AM4378, when DCDC2 FB is tied to VDD_MPU_MON PMIC shuts itself down due to overvoltage. However, when we tie the FB to the output of DCDC2 directly it works fine. See below image for when its tied to VDD_MPU_MON.. Purple line is the MPU voltage and green is the current.
So we started to believe that the VDD_MPU_MON is not working as it should in AM4378 processor in our batch or in general. We would like to know if you can populate this problem in your environment.
Also, we need to know if this situation may have caused any damage to hardware (MPU, DDR, etc.) because we are having some issues with DDR on these boards now after the voltage issues has been resolved with direct connection of FB to DCDC2 output.
Thank you in advance for your quick responses.