This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a question about connecting a serial NOR Flash to SPI0 and booting the device.
The CPU and CSx are connected as follows.
・CS0 - Serial NOR Flash
・CS1-RTC
At this time, RTC's CS is active high, so I would like to fix CS1 to L during startup. Is there any way to do this?
Currently, it is H for about 30ms from power-on until CS1 is set to L by the bootloader.
I can also send the schematic via private message if n
Thanks,
Astro
Hello Astro,
Thank you for the Query.
I can have a look at the schematics to understand the query better.
Is you query on the hardware connection or the software changes.
Regards,
Sreenivasa
Hello Astro,
Can you please reply the above query. I copied the same below
Is you query on the hardware connection or the software changes.
Regards,
Sreenivasa
Hello Astro
I had a quick look at the issues you mentioned and the circuit diagram.
The inputs could be floating during powerup causing this issue.
Can you please try terminating the CS using a resistor.
Regards,
Sreenivasa
Hi, Sreenivasa
Do you mean "place an external pull-down resistor"? If so, I would like to know about:
1. Is it not possible to pull down in the SOC?
2. External pull-down resistor value
Thanks,
Astro
Hello Astro
2. External pull-down resistor value
If it is required to be pulled down during power-up, an external termination is expected to be used.
Regards,
Sreenivasa
Hello Astro
i have not heard from you and closing the thread.
Regards,
Sreenivasa