This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Connecting a serial NOR Flash to SPI0 and booting the device

Guru 10740 points
Part Number: AM3352

Hi,

I have a question about connecting a serial NOR Flash to SPI0 and booting the device.

The CPU and CSx are connected as follows.
・CS0 - Serial NOR Flash
・CS1-RTC

At this time, RTC's CS is active high, so I would like to fix CS1 to L during startup. Is there any way to do this?

Currently, it is H for about 30ms from power-on until CS1 is set to L by the bootloader.

I can also send the schematic via private message if n

Thanks,

Astro