Hi,
According to TRM (SPRUIM2D) section 12.3.5.1.2 "MMCSD Not Supported Features", HS400 DDR is not supported.
But it seems u-boot and Linux kernel recognizes mmc as HS400.
u-boot log:
=> mmcinfo Device: mmc@fa10000 Manufacturer ID: 13 OEM: 14e Name: S0J56 Bus Speed: 200000000 Mode: HS400 (200MHz)
Kernel log:
[ 2.661436] mmc1: new HS400 MMC card at address 0001
My customer wants to know how to limit speed rate up to HS200 in case HS400 eMMC device is connected, both in u-boot and kernel.
Thanks and regards,
Koichiro Tashiro