Part Number: TDA4VM
Hello, TI:
We are developing a custom platform with a TDA4 SoC.
Processor SDK version: 08_01_00_13


phy-mode = "rgmii-id";
phy-handle = <&phy0>;
};
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hello, TI:
We are developing a custom platform with a TDA4 SoC.
Processor SDK version: 08_01_00_13


Regards.
Hi,
Not sure if this is the cause but CPSW MAC only support Rx internal delay mechanism while "rgmii-id" is for adding internal delay in both tx and rx.
Can you try with phy-mode = "rgmii-rxid"
Regards,
Tanmay
Hi,TI
We found that the clock of RGMII TX is 120MHz instead of 125 MHz, and it is generated by soc.
Can you tell us what clock does the RGMII TXC reference?
How can we get clock tree tool of TDA4, and how can we get the clock frequencies report of soc, do you some instructions?
Regards.
Hi,
You can use `k3conf` utility to check clocks set-up on board during run-time. run `k3conf --help` for help on how to use the tool.
For dumping the clocks for mcu_cpsw, you can use this command : ` k3conf dump clock 18`
For details on clocks and devices on TDA4VM, you can see this page.
Regards,
Tanmay
Hi,
Thanks for your reply.
We found that the default PLL value of MCU_CPSW (PLLFRAC2_SSMOD_16FFT_MCU_2) is wrong.Our input crystal Frequency is 19.2 MHz, but the default PLL configurations is set as table of 20Mhz input crystal frequency.
We noticed that "The crystal frequency is understood by the ROM from the BOOTPINS" in TISCI documents(https://software-dl.ti.com/tisci/esd/latest/5_soc_doc/j721e/pll_data.html), so what the BOOTPINS means?
We think some errors occurs when ROM understands the crystal frequency.
Regards.