This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, we are developing a custom platform with a main TDA4 SoC.
Processor SDK version: 06_02_00 (we are planing to upgrade to latest 7_0x_xx in the next phase of development)
On our platform we have connected Marvell 88E1512 Ethernet PHY to MCU_CPSW, Ethernet works fine for 10Mbps and 100Mbps link, but we are having issues to establish 1Gbps link.
Here is our modification of Linux device tree:
Hi Uros,
Re-opening this thread after a long time. Apologies.
Are you still facing this issue or did you find a solution ?
Regards
Vineet