Other Parts Discussed in Thread: SYSCONFIG
Hi experts,
My customer wants to set GPMC's a1 port to C5 pin.
My customer wants to set GPMC's a1 port to C5 pin. However, when the a1 port is set to the C5 pin using the Sysconfig tool, the D8 pin of the a27 port conflicts as shown in the figure below. Since I have not set any ports other than GPMC, there is no port that conflicts with the D8 pin. However, this setting will result in a conflict error. Why is this error printed?
Attach the .syscfg file for this configuration:GMPC_custom.zip
If they set the GPMC's a1 port to the A21 pin, no error will be printed as below.
Attach the .syscfg file for this configuration:GPMC_Default.zip
The sysconfig tool version is "sysconfig_1.14.0"
Best regards,
Sasaki