Our customer wants to use SD card and eMMC and USB flash drive for AM62x and wants to know what is the maximum size supported by RBL (ROM bootloader) for each of the devices.
Does USB MSC boot support a USB flash drive with FAT32?
What is the maximum size supported in Filesystem mode for each of the devices with FAT32? Is it 2 TB?
What is the maximum size supported in Raw Mode for each of the devices? Is it 2 TB?
If these maximum sizes have not been validated, then the theoretical maximum sizes would be acceptable.
Best regards,
Daisuke