This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: ERROR: Running TIDL graph ... Failed !!!

Genius 13655 points

Part Number: TDA4VM

Hello Champs,


Customer ran below model which has been compiled on PC (provided by TI) on sk-tda4m. 

/opt/edgeai-tidl-tools/examples/osrt_python/ort# python3 onnxrt_ep.py

It prompted below error message.

ERROR: Running TIDL graph ... Failed !!!                                       
 17797.921622 s:  VX_ZONE_ERROR:[ownContextSendCmd:815] Command ack message re1
 17797.921649 s:  VX_ZONE_ERROR:[ownContextSendCmd:851] tivxEventWait() failed.
 17797.921670 s:  VX_ZONE_ERROR:[ownNodeKernelInit:538] Target kernel, TIVX_CMe
 17797.921676 s:  VX_ZONE_ERROR:[ownNodeKernelInit:539] Please be sure the tare
 17797.921682 s:  VX_ZONE_ERROR:[ownNodeKernelInit:540] If the target callbackl
 17797.921691 s:  VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for n!
 17797.921699 s:  VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed   
 17797.921704 s:  VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed       
 17797.921804 s:  VX_ZONE_ERROR:[ownGraphScheduleGraphWrapper:820] graph is nod
 17797.921810 s:  VX_ZONE_ERROR:[vxProcessGraph:755] schedule graph failed     
 17797.921816 s:  VX_ZONE_ERROR:[vxProcessGraph:760] wait graph failed         
ERROR: Running TIDL graph ... Failed !!!                                       
 17798.056295 s:  VX_ZONE_ERROR:[ownContextSendCmd:815] Command ack message re1
 17798.056321 s:  VX_ZONE_ERROR:[ownContextSendCmd:851] tivxEventWait() failed.
 17798.056343 s:  VX_ZONE_ERROR:[ownNodeKernelInit:538] Target kernel, TIVX_CMe
 17798.056349 s:  VX_ZONE_ERROR:[ownNodeKernelInit:539] Please be sure the tare
 17798.056355 s:  VX_ZONE_ERROR:[ownNodeKernelInit:540] If the target callbackl
 17798.056363 s:  VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for n!
 17798.056372 s:  VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed   
 17798.056378 s:  VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed       
 17798.056481 s:  VX_ZONE_ERROR:[ownGraphScheduleGraphWrapper:820] graph is nod
 17798.056487 s:  VX_ZONE_ERROR:[vxProcessGraph:755] schedule graph failed     
 17798.056493 s:  VX_ZONE_ERROR:[vxProcessGraph:760] wait graph failed         
ERROR: Running TIDL graph ... Failed !!!                                       
                                                                               
Saving image to  ../../../output_images/                                       
                                                                               
                                                                               
Completed_Model :     4, Name : od-ort-ssd-lite_mobilenetv2_fpn                
                                                                               
                                                                               
 17798.065289 s:  VX_ZONE_INIT:[tivxHostDeInitLocal:100] De-Initialization Don!
 17798.069637 s:  VX_ZONE_INIT:[tivxDeInitLocal:193] De-Initialization Done !!!
APP: Deinit ... !!!                                                            
REMOTE_SERVICE: Deinit ... !!!                                                 
REMOTE_SERVICE: Deinit ... Done !!!                                            
IPC: Deinit ... !!!                                                            
IPC: DeInit ... Done !!!                                                       
MEM: Deinit ... !!!                                                            
MEM: Alloc's: 8 alloc's of 5224020 bytes                                       
MEM: Free's : 8 free's  of 5224020 bytes                                       
MEM: Open's : 0 allocs  of 0 bytes                                             
MEM: Deinit ... Done !!!                                                       
APP: Deinit ... Done !!!

Thanks
Rgds
Shine

  • Hello Shine,

    May i know which SDK version are you seeing this issue?

    Is the model compiled for the respective SDK version?

    Could you enable the remote core logs too by running ./vx_app_arm_remote_log.out &
    and then running the application?

    Could you share these logs too? (i.e., with remote core logs)

    Regards,
    Nikhil

  • Hi Nikhil,

    The SDK version is 
    j7-evm-08_00_00_08. 

    The model is tidl_j721e_08_02_00_11

    log:

    [C7x_1 ]  16164.751710 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16164.751710 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16164.929947 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16164.929947 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.054004 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.054004 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.177258 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.177258 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.300541 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.300541 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.424396 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.424396 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.547571 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.547571 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.670806 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.670806 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.794147 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.794147 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.917320 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16165.917320 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.040791 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.040791 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.164247 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.164247 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.287202 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.287202 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.410429 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.410429 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.533615 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.533615 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.657004 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.657004 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.780401 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.780401 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.903545 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16166.903545 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.026896 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.026896 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.150201 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.150201 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.273668 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.273668 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.396877 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.396877 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.520506 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.520506 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.643761 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.643761 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.766775 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.766775 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.893770 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16167.893770 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.017422 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.017422 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.141036 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.141036 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.264439 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.264439 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.387682 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.387682 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.510974 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.510974 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.634500 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.634500 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.757948 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.757948 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.881158 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16168.881158 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.004770 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.004770 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.128101 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.128101 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.252199 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.252199 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.375376 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.375376 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.498736 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.498736 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.621929 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.621929 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.745560 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.745560 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.869004 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.869004 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.992214 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16169.992214 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.115378 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.115378 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.238854 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.238854 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.361917 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.361917 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.485317 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.485317 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.608510 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.608510 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.731794 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.731794 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.854828 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.854828 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.978318 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16170.978318 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.101475 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.101475 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.225162 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.225162 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.348288 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.348288 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.471441 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.471441 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.594751 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.594751 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.721135 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.721135 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.844221 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.844221 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.967668 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16171.967668 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.091022 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.091022 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.214429 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.214429 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.337679 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.337679 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.461149 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.461149 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.584285 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.584285 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.707512 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.707512 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.830815 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.830815 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.953940 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16172.953940 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.077150 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.077150 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.200351 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.200351 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.323726 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.323726 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.447099 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.447099 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.570368 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.570368 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.693607 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.693607 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.816787 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.816787 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.940341 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16173.940341 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.063432 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.063432 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.186822 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.186822 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.309864 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.309864 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.433340 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.433340 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.556492 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.556492 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.679848 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.679848 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.803046 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.803046 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.926478 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16174.926478 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.049804 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.049804 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.172788 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.172788 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.296032 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.296032 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.419465 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.419465 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.542895 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.666306 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.666306 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.789515 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.789515 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.912515 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16175.912515 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.035610 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.035610 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.158962 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.158962 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.282203 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.282203 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.405813 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.405813 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.529098 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.529098 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.652436 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.652436 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.775786 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.899111 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16177.022192 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16177.145576 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.775786 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.775786 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16176.899111 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16177.022192 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21
    [C7x_1 ]  16177.145576 s:  VX_ZONE_ERROR:[tivxKernelTIDLCreate:644] Network version - 0x21



    Thanks
    Rgds
    Shine

  • Hi Shine,

    This error occurs when you are using the model that is generated for different SDK version

    Since you are using SDK 8.0, please import the model for the same SDK 8.0 where the expected version is 0x20210723

    Regards,
    Nikhil

  • Hi Nikhil,

    Thanks for your support.

    Below is the customer's reply.

    Sorry that I misunderstood the sdk version.  In the 08.02 document, it is said that “If you wish to work with just the Edge AI Applications, you can edit-build-run directly on the target by flashing the etcher image as specified in Preparing SD card image.", so I used 08.02 image. The model compiled on PC is based on https://github.com/TexasInstruments/edgeai-tidl-tools/blob/master/examples/osrt_python/README.md#model-compilation-on-pc. 

    Will the content in the link be updated in future? I find 08.02 and 08.04 use the same link. If the link will be updated later, which is the link for 08.02?

    Thanks.
    Rgds
    Shine

  • Hello Shine,

    I shall loop in a TIDL expert to respond to this query.

    Regards,
    Nikhil

  • Hi Shine,

    you can find all versions of releases in below link
    PROCESSOR-SDK-LINUX-SK-TDA4VM Software development kit (SDK) | TI.com on the left pane

    Below is the link for 8.2
    https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-SK-TDA4VM/08.02.00.02

    Regards
    Rahul T R