Hello TI team:
I'm a engineer of valeo, I'm currently developing a project based on the am62x chip. At present, we need to do development work based on the am62x R5 core. I got the mcu-sdk(mcu_plus_sdk_am62x_08_05_00_15) and imported to CCS. I compiled an image of am62-mcu-r5f0_0-fw and put it in the /lib/firmware path. then I run the command echo start > /sys/class/remoteproc0/state,but I didn't find that the r5 image was executed.
Does the R5 FW image work like this? can you support me ?