Dear TI Support,
After I run the /etc/init.d/rc.pvr start command to initialize the GPU, I am getting a few error messages printed to the screen:
root@tqma65xx-2gb-mba65xx:/etc/init.d# ./rc.pvr start PVR:(Error): PVRSRVDetectPlaform: Unknown platform: TQ-Systems���. [0, ] PVR:(Error): PVRSRVDetectPlaform: Unknown platform: TQ-Systems]���. [0, ] PVR:(Error): SGXInitialisePart1: Could not get core count from platform. Using 1 [0, ] Loaded PowerVR consumer services.
The one that concerns me the most is that it states it is only using one core. What can I do to help it detect my platform and also detect the correct number of cores to use?
Here is the output of gfx_check.sh which provides some information about my setup:
root@tqma65xx-2gb-mba65xx:~# ./gfx_check.sh WSEGL settings [default] WindowSystem=libpvrQWSWSEGL.so ------ ARM CPU information processor : 0 BogoMIPS : 400.00 Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid CPU implementer : 0x41 CPU architecture: 8 CPU variant : 0x0 CPU part : 0xd03 CPU revision : 4 processor : 1 BogoMIPS : 400.00 Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid CPU implementer : 0x41 CPU architecture: 8 CPU variant : 0x0 CPU part : 0xd03 CPU revision : 4 processor : 2 BogoMIPS : 400.00 Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid CPU implementer : 0x41 CPU architecture: 8 CPU variant : 0x0 CPU part : 0xd03 CPU revision : 4 processor : 3 BogoMIPS : 400.00 Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid CPU implementer : 0x41 CPU architecture: 8 CPU variant : 0x0 CPU part : 0xd03 CPU revision : 4 ------ SGX driver information Version SGX_DDK sgxddk 1.17@4948957 (release) omap_linux System Version String: SGX revision = 117 ------ Framebuffer settings ------ Rotation settings 0 ------ Kernel Module information Module Size Used by pvrsrvkm 720896 0 hid_multitouch 327680 0 usbhid 327680 0 xhci_plat_hcd 327680 0 xhci_hcd 393216 1 xhci_plat_hcd usbcore 458752 3 xhci_hcd,usbhid,xhci_plat_hcd crct10dif_ce 262144 1 dwc3 327680 0 udc_core 262144 1 dwc3 usb_common 262144 5 xhci_hcd,usbcore,xhci_plat_hcd,dwc3,udc_core tidss 327680 0 videobuf2_dma_contig 262144 1 tidss videobuf2_memops 262144 1 videobuf2_dma_contig v4l2_mem2mem 262144 1 tidss videobuf2_v4l2 262144 2 tidss,v4l2_mem2mem videobuf2_common 327680 3 videobuf2_v4l2,tidss,v4l2_mem2mem phy_omap_usb2 262144 4 dwc3_keystone 262144 0 sch_fq_codel 262144 3 fuse 393216 1 ipv6 720896 32 ------ Boot settings root=/dev/mmcblk1p2 rw rootfstype=ext4 rootwait earlycon=ns16550a,mmio32,0x02800000 console=ttyS2,115200n8 ------ Linux Kernel version Linux tqma65xx-2gb-mba65xx 5.4.109-rt55 #1 SMP PREEMPT_RT Mon Feb 21 09:29:21 UTC 2022 aarch64 aarch64 aarch64 GNU/Linux
Thanks!
Joseph Keene