Is the 9-bit operation mode for the UART available in Linux and supported by existing drivers?
Thank you in advance
--
Olof
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the 9-bit operation mode for the UART available in Linux and supported by existing drivers?
Thank you in advance
--
Olof
Hi Olof,
The Linux kernel driver does NOT support the 9-bit UART operation mode.
#define UART_LCR_WLEN5 0x00 / Wordlength: 5 bits /
#define UART_LCR_WLEN6 0x01 / Wordlength: 6 bits /
#define UART_LCR_WLEN7 0x02 / Wordlength: 7 bits /
#define UART_LCR_WLEN8 0x03 / Wordlength: 8 bits */
The above lengths are supported.
Best Regards,
Keerthy
Thank you Keerthy, is this because of a hardware limitation or a software limitation?
What would it take to make the linux driver operate in 9-bit mode?
We would need the 9th bit only to flag/frame new packets, if that help find a solution.
Olof,
Okay. To make a distinction the hardware does support but there is no software support for this mode. Currently there is no plans of adding this.
Best Regards,
Keerthy