hi all
in our custom board based on am4372, we have a spi0 interface to rtc. in uboot 2022.01 which I ported spi0 interface is working fine . but in linux is was not working. why diagnosing I found the PRCM_CLKCTRL the value is 00300000. that means it is disabled.
why it is so?
I have made the status=okay for spi0 in dts.
there is absolutely no problem with pinmux or hardware as it tested on uboot
also I have notices while booting for some module ti,sysc probe fails with error -16.
I think both are related issue.
can anybody throw light on this?