Hi,
Let me ask a quick question.
I am using 3 kind of C66x DSP: C6655/54/52,and I downloaded the ROM code for C6655/57 in order to understand RBL behavior.
RBL code is available from the following link:
https://software-dl.ti.com/sdoemb/sdoemb_public_sw/rbl/1_0_C6657/index_FDS.html
I'm reading the code because I need to understand spi boot, but some codes seems to have been modified.
For example, please take a look at chipInitStatusReg() function at Gauss.c.
Judging from the actual operation of RBL, chipKickUnlock() and chipKickLock() seems to be removed from this function at present.
I read RBL version from C6655/54 chip,the RBL version is v01.00.00.04.Tue.Dec.06.18:24:48.2011.
How can I get v01.00.00.04 RBL source code?
Best Regards,
AnnaWang