Part Number: PROCESSOR-SDK-AM64X
Dear TI Engineers and Experts,
I am configuring my AM64x Start Kit with the Wi-SUN software on it and they are working well.
https://www.ti.com/tool/SK-AM64
PROCESSOR-SDK-LINUX-AM64X — Processor SDK Linux for AM64x
Version: 08.05.00.21
Release date: 14 Dec 2022
Then, I continue my journey by plugging in an USB powering mobile LTE dialup modem onto my AM64X Start Kit board.
This modem did show up when I issued command:
lsusb
also when I issued command lsmod, I saw these modules were loaded:
usb_wwan
In order to configure my lte modem to function, I still need qmi_wwan and also the Linux Network Manager and/or Modem Manager binary which is named as
nmcli and so on.
Can you suggest a simple so that I can include Network Manager and Modem Manager binaries into my AM64x Start Kit SD card image.
Yours faithfully,
Timmy