Other Parts Discussed in Thread: ADC3221
ADC3221 has serial LVDS interface with bit clock and frame clock, but OMAP-L138 does not have LVDS, but it has many interfaces. So which interface shall I use to connect them? Is there extra bridging chip/circuit needed?
For the ADC part, sampling rate will be 25Msps for 2 channels, 12bit resolution, therefore data rate for each channel at least 25*12 = 300 bit/s.
For OMAP-L138,
It has SATA interface that use LVDS signaling, but its one clock, one transmit, one receive lines do not match the LVDS lines of ADC3221 (one bit clock, one frame clock, one or two data output).