I have an SK-AM68 Starter kit which I am trying to connect to via the provided USB Cable (Type-A to Micro-B) but I am not able to get any output so far.
I am using a POWERPAX USB-C 72W device which I have read supports USB-C Power Delivery which should be capable of outputting 20V at 3A. And I have read in the starter guide that the USB Type C connection has Power Delivery 3.0 support. I am using a USB-C to USB-C cable rated at 100W. So I believe there should be enough power to the board.
And I have connected the Micro-B USB cable in J4 on the board and then into my host PC.
The power LED (LD2) has lit up red, and so has the UART-over-USB LED (LD1).
After connecting the USB I get four devices: /dev/ttyUSB0 /dev/ttyUSB1 /dev/ttyUSB2 /dev/ttyUSB3
I have downloaded the tisdk-edgeai-image-j721s2-evm.wic.xz image and placed it onto the sd card after extracting it and using BalenaEtcher. You can see the contents here:
'System Volume Information' tispl.bin uEnv.txt.base tiboot3.bin u-boot.img version tiboot3-j721s2-gp-evm.bin uEnv_edgeai-apps.txt tiboot3-j721s2-hs-fs-evm.bin uEnv.txt
I have inserted the SD card and I have ensured the boot pins are set to all OFF so it should boot from SD card.
I connect with picocom to /dev/ttyUSB2 with a baud rate of 115200 and i turn the board on and off again and I get no output at all in my terminal. And I cannot input anything as if it was stuck on the uboot shell.
I have also tried to see if there was any output from the HDMI port but I don't get any image when I do that.
Things I have tried:
- Using mksdboot.sh from the ti-processor-sdk-linux to create another sd card rather than the supplied one.
- I have connected the board via Ethernet to my host PC and used wireshark to check any transmissions from the board and there seems to be packets coming from the device.
- I have tried using Tera Term on windows after installing the listed required driver to connect to all four COM ports with baud rate 115200 and again no output.
- Using other programs e.g. minicom over picocom,
- Showing output from all /dev/ttyUSB* devices
- Using a different micro USB cable
- Trying to power through a usb-c cable from my host pc to the board
I have tried connecting on host Pc of Ubuntu 22.04 and Windows 10.
My experience is mostly with software rather than hardware but from my use of theTMDSEVM572x board I should be getting some boot log output. I am a little unsure on what to try next or if I have missed something fundamental.
Any advice on what to try next would be appreciated