Hi team,
The customer want to implement key polling and interrupts on the AM5708 DSP core refer to the code configuration of the SDK. But it failed.
As the following code: the LED output toggles normally, but neither key detection works:
/** * \file tl-led-flash.c * * \brief Example application main file. This application will toggle the led. * The led toggling will be done inside an callback function, which * will be called by Interrupt Service Routine. Interrupts are * triggered manually and no external source is used to trigger * interrupts. * * \version 1.0 */ /* XDCtools Header files */ #include <xdc/std.h> #include <xdc/cfg/global.h> #include <xdc/runtime/System.h> #include <xdc/runtime/Error.h> /* BIOS Header files */ #include <ti/sysbios/BIOS.h> #include <ti/sysbios/knl/Task.h> #include <stdio.h> #include <string.h> /* TI-RTOS Header files */ #include <ti/drv/gpio/GPIO.h> #include <ti/drv/gpio/soc/GPIO_soc.h> /* UART Header files */ #include <ti/drv/uart/UART.h> #include <ti/drv/uart/UART_stdio.h> #include <ti/drv/uart/test/src/UART_board.h> #include <ti/board/board.h> #include <ti/csl/soc.h> #include <ti/csl/soc/am572x/src/cslr_control_core_pad_io.h> #include <ti/board/src/evmAM572x/include/evmam572x_pinmux.h> /********************************************************************** ************************** Macros ************************************ **********************************************************************/ #define GPIO_PIN_VAL_LOW (0U) #define GPIO_PIN_VAL_HIGH (1U) #define GPIO_USER0_LED_PIN_NUM (0x04U) #define GPIO_USER0_LED_PORT_NUM (0x04) /* user-led0, gpio4_4 */ #define GPIO_USER1_LED_PIN_NUM (0x04U) #define GPIO_USER1_LED_PORT_NUM (0x05) /* user-led1, gpio5_4 */ #define GPIO_USER2_LED_PIN_NUM (0x05U) #define GPIO_USER2_LED_PORT_NUM (0x05) /* user-led2, gpio5_5 */ #define GPIO_USER_KEY3_PIN_NUM 5 #define GPIO_USER_KEY3_PORT_NUM 4 //GPIO4_5 #define GPIO_USER_KEY4_PIN_NUM 20 #define GPIO_USER_KEY4_PORT_NUM 6 //GPIO6_20 /********************************************************************** ************************** Internal functions ************************ **********************************************************************/ /* GPIO Driver board specific pin configuration structure */ GPIO_PinConfig gpioPinConfigs[] = { GPIO_DEVICE_CONFIG(GPIO_USER0_LED_PORT_NUM, GPIO_USER0_LED_PIN_NUM) | GPIO_CFG_OUTPUT, GPIO_DEVICE_CONFIG(GPIO_USER1_LED_PORT_NUM, GPIO_USER1_LED_PIN_NUM) | GPIO_CFG_OUTPUT, GPIO_DEVICE_CONFIG(GPIO_USER2_LED_PORT_NUM, GPIO_USER2_LED_PIN_NUM) | GPIO_CFG_OUTPUT, GPIO_DEVICE_CONFIG(GPIO_USER_KEY3_PORT_NUM, GPIO_USER_KEY3_PIN_NUM) | GPIO_CFG_INPUT, GPIO_DEVICE_CONFIG(GPIO_USER_KEY4_PORT_NUM, GPIO_USER_KEY4_PIN_NUM) | GPIO_CFG_IN_INT_RISING | GPIO_CFG_INPUT }; /* GPIO Driver call back functions */ GPIO_CallbackFxn gpioCallbackFunctions[] = { NULL, NULL, NULL, NULL, NULL }; /* GPIO Driver configuration structure */ GPIO_v1_Config GPIO_v1_config = { .pinConfigs = gpioPinConfigs, .callbacks = gpioCallbackFunctions, .numberOfPinConfigs = sizeof(gpioPinConfigs) / sizeof(GPIO_PinConfig), .numberOfCallbacks = sizeof(gpioCallbackFunctions) / sizeof(GPIO_CallbackFxn), .intPriority = 20, }; /* ON Board LED pins which are connected to GPIO pins. */ typedef enum GPIO_LED { USER_LED0 = 0, USER_LED1, USER_LED2, END }GPIO_LED; typedef enum GPIO_INPUT { USER_KEY3 = 3, USER_KEY4 = 4 }GPIO_INPUT; void print_debug(char *str) { UART_puts(str,strlen(str)); } void user_key3_cb(void) { print_debug("\n user_key3_cb \n"); } void user_key4_cb(void) { print_debug("\n user_key4_cb \n"); } void GPIO_PIN_MUX(void) { uint32_t regVal = 0; /* GPIO pinmux configuration */ CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D3_VIN2A_D3_MUXMODE, 0xEU); ((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_VIN2A_D3 = regVal; /* vin2a_d3.gpio4_4(user_led0) */ CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_MCASP1_AXR2_MCASP1_AXR2_MUXMODE, 0xEU); ((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_MCASP1_AXR2 = regVal; /* mcasp1_axr2.gpio5_4(user_led1) */ CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_MCASP1_AXR3_MCASP1_AXR3_MUXMODE, 0xEU); ((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_MCASP1_AXR3 = regVal; /* mcasp1_axr3.gpio5_5(user_led2) */ CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D4_VIN2A_D4_MUXMODE, 0xEU); ((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_VIN2A_D4 = regVal; /* VIN2A_D4.gpio4_5(user_key3) */ CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_XREF_CLK3_XREF_CLK3_MUXMODE, 0xEU); ((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_XREF_CLK3 = regVal; /* XREF_CLK3.gpio6_20(user_key4) */ /* GPIO4 Clock Enable */ *(unsigned int*)0x4A009770 = (unsigned int)(0x00000102); /* GPIO6 Clock Enable */ *(unsigned int*)0x4A009780 = (unsigned int)(0x00000102); // /* Set the callback function */ // GPIO_setCallback(USER_KEY3, user_key3_cb); // /* Enable GPIO interrupt on the specific gpio pin */ // GPIO_enableInt(USER_KEY3); /* Set the callback function */ GPIO_setCallback(USER_KEY4, user_key4_cb); /* Enable GPIO interrupt on the specific gpio pin */ GPIO_enableInt(USER_KEY4); } /* * ======== Board_initGPIO ======== */ static void Board_initGPIO(void) { Board_initCfg boardCfg; boardCfg = BOARD_INIT_MODULE_CLOCK | BOARD_INIT_UART_STDIO; Board_init(boardCfg); } /********************************************************************** ************************** Global Variables ************************** **********************************************************************/ /* * ======== task function ======== */ void tl_led_flash(UArg arg0, UArg arg1) { uint8_t i = 0; /* GPIO initialization */ GPIO_init(); GPIO_PIN_MUX(); print_debug("\n GPIO Led Blink Application \n"); while(1) { /* Turn on LEDs */ for ( i = 0; i < END; i++ ){ GPIO_write(i,GPIO_PIN_VAL_HIGH); } /* Keep the LEDs on for 500 ms */ Task_sleep(500); /* Turn off LEDs */ for ( i = 0; i < END; i++ ){ GPIO_write(i,GPIO_PIN_VAL_LOW); } /* Keep the LEDs off for 500 ms */ Task_sleep(500); if(GPIO_read(USER_KEY3) == 1) { print_debug("key3 is press\n"); } if(GPIO_read(USER_KEY4) == 0) { print_debug("key4 is press\n"); } } Task_exit(); } /* * ======== main ======== */ int main(void) { Task_Handle task; Error_Block eb; Error_init(&eb); /* Call board_init functions */ Board_initGPIO(); /* create a Task, which is tl_led_flash */ task = Task_create(tl_led_flash, NULL, &eb); if (task == NULL) { System_printf("Task_create() failed!\n"); BIOS_exit(0); } /* Start BIOS */ BIOS_start(); return (0); }
Could you help check this case? Thanks.
Best Regards,
Cherry