This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: DDR ECC Example for Cortex-R5

Part Number: AM6548

Hello,

Within the PDK for the AM6548, is there an CSL ECC example or test for DDR? It seems that the examples that come with the PDK are only for AM64x, SOC_J721E, or SOC_J7200. The ECC DDR examples under C:\ti\pdk_am65xx_08_02_00_21\packages\ti\csl\example\ecc\ecc_test_app are not compatible with AM65x PDK it seems. 

  • Hi 

    The AM65 PDK / RTOS SDK is limited support and provided as is. There are no plans to add any new examples/content to this. There are no plans for bug fixes either. 

    We are planning to offer a limited functionality MCU+ SDK which will be closer to our AM64x offering but without any RTOS side drivers for display, USB, PCIE, CPSW LWiP etc , this is slated for end of this year. 

    Regards

    Mukul 

  • Thanks for replying Mukul, do you have any suggestions on porting the example from the PDK within ti/csl/example/ecc/ecc_test_app/ecc_ddr.c for AM65x_GP_EVM ? There are some API differences in the CSL functions within this example and some guidance would be appreciated