Other Parts Discussed in Thread: CSD
Hi,
We have been trying to boot from the eMMC on the AM4376(GP). We have not been successful in getting a stable MLO to run and output debug printouts. We have been successful with an SD card with the same partition scheme in FAT32 mode.
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
mmcblk0 179:0 0 29.8G 0 disk
|-mmcblk0p1 179:1 0 128M 0 part /run/media/mmcblk0p1
`-mmcblk0p2 179:2 0 3.9G 0 part /
mmcblk1 179:16 0 14.8G 0 disk
|-mmcblk1p1 179:17 0 128M 0 part /run/media/mmcblk1p1
`-mmcblk1p2 179:18 0 3.9G 0 part /run/media/mmcblk1p2
mmcblk1boot0 179:32 0 31.5M 1 disk
mmcblk1boot1 179:48 0 31.5M 1 disk
(Partition 1 is FAT32 and partition 2 is .ext3)
The Sysboot setup is SYSBOOT[4:0] = 10100 to default to eMMC when there is no SD card.
We wait for all boot sources to cycle but we do not see any debug printouts.
When booting from alternate source we can access the eMMC in mmcblk1 as shown above.

(eMMC Schematic)

(AM4376 eMMC Schematic)
We have removed DS from the board as we have seen in previous conversation that was recommended to be left floating for eMMC 4.5( to disable 5.x)
Please advise.
Thank you!