We have received our first boards and work on the bring up. Review has been done prior to production by TI and necessary modifications has been considered. Compared to the EVM we use a different DDR4 and plan to use USB Boot. At the moment we face the following issues:
- JTAG - we do have basic connection to SOC, however, we cannot connect to any Core
- USB Boot - My PC recognizes the device and I can also start a transfer, but then there is an immediate reset. And it's not a HW reset (the line between PMCI and AM62A stays high). So apparently the boot ROM starts, but then the SoC is resetting.
So what kind of verification we can do? What are the minimum requirements to have USB boot working? (DDR init, Voltages, Sequence, clock, ...)