HI,
Is it possible to use an RMII PHY with the AM6548 processor and use it as an EtherCAT slave? The EtherCAT slave demo for the TMD654IDEVM board has explicit instructions to modify the board to change the PHY from RGMII to MII mode. The EVM board is using DP83867IRPAPT PHY which has a 64-pin package, but for layout reasons, we would like to go with a 48-pin package such as the DP83867CRRGZ if possible.
Thanks,
Robert