Other Parts Discussed in Thread: AM62P
Hello Experts,
In the TRM, there is following description
>These bits do not apply to "I2C OD FS" buffer types as these IOs do not have internal pull registers.
>The MCU_I2C0 and WKUP_I2C0 IOs are a special IIC Open Drain Cell I2C_OD_FS.
- What is "FS"?
- Will only the two I2C have the internal pull setting disabled while the other I2C have the internal setting enabled?
Best regards,
Ken