Other Parts Discussed in Thread: TDA2, MMWCAS-DSP-EVM
I am using MMWCAS-DSP-EVM and want to program the DSP inside TDA2. I can connect the A15 with no problem but not the DSPs.How to connect DSP using JTAG/?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using MMWCAS-DSP-EVM and want to program the DSP inside TDA2. I can connect the A15 with no problem but not the DSPs.How to connect DSP using JTAG/?
Hello,
I am directing your inquiry to the domain engineer best able to support you.
Best,
Kelvin
Hi Chung,
Can you confirm if you have followed all the steps from section 3.9 of the following document?
PROCESSOR_SDK_RADAR_03_08_00_00/vision_sdk/docs/UserGuides/VisionSDK_UserGuide_TDA2xx.pdf
Regards,
Kaushik
Hi Sir
It is not working for me. Please advice what I can do for next step. Sorry, I do need help on this.
BR
Jack
Hi Chung,
Please find the link below:
https://software-dl.ti.com/sdo/sdo_apps_public_sw/CCSv9/auto_rvp_rsp_device_support_1.1.8.zip
You should get the required GEL files from this package. Alternatively, you can add this product (TDA2) on the latest version of CCS installation as well.
Regards,
Kaushik
Hi Kaushik
It is stil not working for me. I got the message for connection test through CCS12.
[Start: Spectrum Digital XDSPRO USB Emulator]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\jackho\AppData\Local\TEXASI~1\CCS\
ccs1250\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
The library build date was 'Sep 6 2023'.
The library build time was '14:41:42'.
The library package version is '9.13.0.00201'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '6' (0x00000006).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.
A error occurred while attempting to reset the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-128' (0xffffff80).
The title is 'SC_ERR_CMD_INVALID_MULT'.
The explanation is:
Unified-SCIF is operating in multiple client mode.
The operation being attempted is invalid in this mode.
It is likely a problem with `SC_CMD' in SMG_call().
[End: Spectrum Digital XDSPRO USB Emulator]