Part Number: TDA4VM
Hello,
we are developing a custom platform with a main TDA4 SoC.
Processor SDK version: ti-processor-sdk-linux-j7-evm-08_06_01_02.
We are using the NOR FLASH model GD25LX512ME, but it cannot start up. The error log is as follows:
�
U-Boot SPL 2021.01-00001-g256d506167-dirty (Dec 02 2023 - 16:10:08 +0800)
Model: Texas Instruments J721E SK A72-2
--++//->EEPROM not available at 0x57, trying to read at 0x58
Reading on-board EEPROM at 0x58 failed 1
Board: J721EX-PM1-SOM rev E2
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
--++//->EEPROM not available at 0x57, trying to read at 0x58
Reading on-board EEPROM at 0x58 failed 1
Trying to boot from SPI
Loading rproc fw image from device 3 not supported!
Starting ATF on ARM64 core...
ti_sci dmsc@44083000: ti_sci_get_response: Message receive failed. ret = -110
ti_sci dmsc@44083000: Message not acknowledgedFailed to put device 262 (-19)
resetting ...
ti_sci dmsc@44083000: ti_sci_get_response: Message receive failed. ret = -110
ti_sci dmsc@44083000: Message not acknowledgedti-sci-sysreset sysreset-controller: ti_sci_sysreset_request: reboot_device failed (-19)
ti_sci dmsc@44083000: ti_sci_get_response: Message receive failed. ret = -110
ti_sci dmsc@44083000: Message not acknowledgedti-sci-sysreset sysreset-controller: ti_sci_sysreset_request: reboot_device failed (-19)
ti_sci dmsc@44083000: ti_sci_get_response: Message receive failed. ret = -110
ti_sci dmsc@44083000: Message not acknowledgedti-sci-sysreset sysreset-controller: ti_sci_sysreset_request: reboot_device failed (-19)
System reset not supported on this platform
### ERROR ### Please RESET the board ###
Hardware schematic diagram: