Hi,
My customer wants to know the LPDDR4/DDR4 refresh rate on Linux SDK. Could you please answer the following their questions ?
Q1. Is it a fixed value or does it vary depending on the temperature?
Q2. If it is a fixed value, what is it ? where can they check it ?
Q3. If it is different each version of silicon or SDK, please let them know that.
Please answer at least Q1 as soon as possible today in advance if it is difficult to answer all of above questions soon.
They found the part for directly writing registers to the DDR controller in the device tree, but they cannot confirm if it is overwritten by other part somewhere.
Also, they found the following thread on E2E.
There is the following comment on this thread.
- I've been told the dynamic refresh rate feature should be added towards the end of this year.
Will the dynamic refresh rate feature be added in the next version 9.1 of Processor SDK Linux for AM64x ? If so, what’s the schedule ?
Thanks and regards,
Hideaki