Hello TI experts,
We add a local IPC to communicate with A53 core on DM R5F core.
We meet an error when running "source /opt/vision_apps/vision_apps_init.sh" command.
Log as below :
before.txt doesn't add local IPC.
after.txt is added local IPC.
The priority of receive IPC task is set to 3, stack size is set to 128 * 1024.
We can see the IPC communication is create and work well in the after.txt.
[MCU1_0] 13.293364 s: rtosIPCMgrInit: Init ... !!!
[MCU1_0] 13.293414 s: rtosIPCMgrCreateRpmsgRxLinuxTask
[MCU1_0] 13.293576 s: REMOTE_SERVICE: Init ... !!!
[MCU1_0] 27.984385 s: [1] Receive the heart from A53 core IPC!
but we can't see the init done log of remote service module.
We can see the init done log of remote service module in the before.txt.
[MCU1_0] 13.367020 s: REMOTE_SERVICE: Init ... Done !!!
root@am62axx-evm:~# source /opt/vision_apps/vision_apps_init.sh root@am62axx-evm:~# root@am62axx-evm:~# [MCU1_0] 1.087010 s: CIO: Init ... Done !!! [MCU1_0] 1.087068 s: APP: Init ... !!! [MCU1_0] 1.087087 s: MEM: Init ... !!! [MCU1_0] 1.087105 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ af000000 of size 16777216 bytes !!! [MCU1_0] 1.087158 s: MEM: Init ... Done !!! [MCU1_0] 1.087173 s: IPC: Init ... !!! [MCU1_0] 1.087189 s: IPC: 3 CPUs participating in IPC !!! [MCU1_0] 1.087515 s: IPC: Waiting for HLOS to be ready ... !!! [MCU1_0] 1.091986 s: Sciserver Version: v2023.12.0.0-REL.MCUSDK.09.01.00.39+ [MCU1_0] 1.094758 s: ##RM_PM_HAL Version: v09.01.08 [MCU1_0] 1.097705 s: ##Starting Sciserver..... PASSED [MCU1_0] 13.366588 s: IPC: HLOS is ready !!! [MCU1_0] 13.366734 s: IPC: Init ... Done !!! [MCU1_0] 13.366757 s: APP: Syncing with 2 CPUs ... !!! [MCU1_0] 13.366779 s: APP: Syncing with 2 CPUs ... Done !!! [MCU1_0] 13.366799 s: REMOTE_SERVICE: Init ... !!! [MCU1_0] 13.367020 s: REMOTE_SERVICE: Init ... Done !!! [MCU1_0] 13.367044 s: FVID2: Init ... !!! [MCU1_0] 13.367073 s: FVID2: Init ... Done !!! [MCU1_0] 13.367090 s: VHWA: VPAC Init ... !!! [MCU1_0] 13.367105 s: SCICLIENT: Sciclient_pmSetModuleState module=219 state=2 [MCU1_0] 13.367194 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU1_0] 13.367218 s: VHWA: LDC Init ... !!! [MCU1_0] 13.367324 s: VHWA: LDC Init ... Done !!! [MCU1_0] 13.367345 s: VHWA: MSC Init ... !!! [MCU1_0] 13.367675 s: VHWA: MSC Init ... Done !!! [MCU1_0] 13.367697 s: VHWA: VISS Init ... !!! [MCU1_0] 13.367793 s: VHWA: VISS Init ... Done !!! [MCU1_0] 13.367908 s: VHWA: VPAC Init ... Done !!! [MCU1_0] 13.367959 s: VX_ZONE_INIT:Enabled [MCU1_0] 13.367977 s: VX_ZONE_ERROR:Enabled [MCU1_0] 13.367993 s: VX_ZONE_WARNING:Enabled [MCU1_0] 13.368883 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:78] Added target MCU1-0 [MCU1_0] 13.369077 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:78] Added target VPAC_LDC1 [MCU1_0] 13.369202 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:78] Added target VPAC_MSC1 [MCU1_0] 13.369368 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:78] Added target VPAC_MSC2 [MCU1_0] 13.369992 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:78] Added target VPAC_VISS1 [MCU1_0] 13.370025 s: VX_ZONE_ERROR:[ownTargetCreate:1217] target is NULL [MCU1_0] 13.370051 s: VX_ZONE_ERROR:[tivxPlatformCreateTargetId:75] Could not Add Target [MCU1_0] 13.370081 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:78] Added target VPAC_VISS1 [MCU1_0] 13.370110 s: VX_ZONE_ERROR:[ownTargetCreate:1217] target is NULL [MCU1_0] 13.370135 s: VX_ZONE_ERROR:[tivxPlatformCreateTargetId:75] Could not Add Target [MCU1_0] 13.370164 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:78] Added target VPAC_VISS1 [MCU1_0] 13.370193 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU1_0] 13.370214 s: APP: OpenVX Target kernel init ... !!! [MCU1_0] 13.371646 s: Cogent ISP Framework [MCU1_0] 13.371778 s: Build: 4.0.63.1 8a5b292c 2023-07-26T04:24:51Z [MCU1_0] 13.374046 s: [API.INIT] Tweak is not compiled-in [MCU1_0] 13.374095 s: [ISP_TRACE.INIT] Trace is not compiled-in [MCU1_0] 13.377665 s: APP: OpenVX Target kernel init ... Done !!! [MCU1_0] 13.377693 s: VISS REMOTE SERVICE: Init ... !!! [MCU1_0] 13.377723 s: VISS REMOTE SERVICE: Init ... Done !!! [MCU1_0] 13.377756 s: APP: Init ... Done !!! [MCU1_0] 13.377774 s: APP: Run ... !!! [MCU1_0] 13.377788 s: IPC: Starting echo test ... [MCU1_0] 13.377811 s: IPC: RecvTask: Creating ... [MCU1_0] 13.377896 s: IPC: RecvTask: Started ... [MCU1_0] 13.377939 s: IPC: SendTask2: Creating ... [MCU1_0] 13.378027 s: IPC: SendTask2: Started ... [MCU1_0] 13.378053 s: IPC: SendTask7: Creating ... [MCU1_0] 13.378137 s: IPC: SendTask7: Started ... [MCU1_0] 13.378163 s: APP: Run ... Done !!! [C7x_1 ] 1.090630 s: CIO: Init ... Done !!! [C7x_1 ] 1.090650 s: APP: Init ... !!! [C7x_1 ] 1.090662 s: SCICLIENT: Init ... !!! [C7x_1 ] 1.090742 s: SCICLIENT: DMSC FW version [9.1.8--v09.01.08 (Kool Koala)] [C7x_1 ] 1.090761 s: SCICLIENT: DMSC FW revision 0x9 [C7x_1 ] 1.090776 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_1 ] 1.090791 s: SCICLIENT: Init ... Done !!! [C7x_1 ] 1.090803 s: UDMA: Init ... !!! [C7x_1 ] 1.090825 s: UDMA: Init ... Done !!! [C7x_1 ] 1.090838 s: MEM: Init ... !!! [C7x_1 ] 1.090850 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ b2000000 of size 117440512 bytes !!! [C7x_1 ] 1.090879 s: MEM: Init ... Done !!! [C7x_1 ] 1.090892 s: IPC: Init ... !!! [C7x_1 ] 1.090904 s: IPC: 3 CPUs participating in IPC !!! [C7x_1 ] 1.091128 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_1 ] 13.358908 s: IPC: HLOS is ready !!! [C7x_1 ] 13.359015 s: IPC: Init ... Done !!! [C7x_1 ] 13.359034 s: APP: Syncing with 2 CPUs ... !!! [C7x_1 ] 13.366780 s: APP: Syncing with 2 CPUs ... Done !!! [C7x_1 ] 13.366801 s: REMOTE_SERVICE: Init ... !!! [C7x_1 ] 13.367961 s: REMOTE_SERVICE: Init ... Done !!! [C7x_1 ] 13.367986 s: VX_ZONE_INIT:Enabled [C7x_1 ] 13.368003 s: VX_ZONE_ERROR:Enabled [C7x_1 ] 13.368016 s: VX_ZONE_WARNING:Enabled [C7x_1 ] 13.368752 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1 [C7x_1 ] 13.368871 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2 [C7x_1 ] 13.368974 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3 [C7x_1 ] 13.369080 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4 [C7x_1 ] 13.369185 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5 [C7x_1 ] 13.369288 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6 [C7x_1 ] 13.369391 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7 [C7x_1 ] 13.369508 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8 [C7x_1 ] 13.369540 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C7x_1 ] 13.369564 s: APP: OpenVX Target kernel init ... !!! [C7x_1 ] 13.369808 s: APP: OpenVX Target kernel init ... Done !!! [C7x_1 ] 13.369832 s: APP: Init ... Done !!! [C7x_1 ] 13.369848 s: APP: Run ... !!!
[MCU1_0] 1.092324 s: CIO: Init ... Done !!! [MCU1_0] 1.092369 s: APP: Init ... !!! [MCU1_0] 1.092384 s: MEM: Init ... !!! [MCU1_0] 1.092400 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ af000000 of size 16777216 bytes !!! [MCU1_0] 1.092440 s: MEM: Init ... Done !!! [MCU1_0] 1.092455 s: IPC: Init ... !!! [MCU1_0] 1.092470 s: IPC: 3 CPUs participating in IPC !!! [MCU1_0] 1.092753 s: IPC: Waiting for HLOS to be ready ... !!! [MCU1_0] 1.093025 s: ##DM Built On: Mar 20 2024 10:25:49 [MCU1_0] 1.098133 s: ##Sciserver Version: v2023.12.0.0-REL.MCUSDK.09.01.00.39+ [MCU1_0] 1.100907 s: ##RM_PM_HAL Version: v09.01.08 [MCU1_0] 1.103853 s: ##Starting Sciserver..... PASSED [MCU1_0] 13.293139 s: IPC: HLOS is ready !!! [MCU1_0] 13.293284 s: IPC: Init ... Done !!! [MCU1_0] 13.293310 s: APP: Syncing with 2 CPUs ... !!! [MCU1_0] 13.293332 s: APP: Syncing with 2 CPUs ... Done !!! [MCU1_0] 13.293364 s: rtosIPCMgrInit: Init ... !!! [MCU1_0] 13.293414 s: rtosIPCMgrCreateRpmsgRxLinuxTask [MCU1_0] 13.293576 s: REMOTE_SERVICE: Init ... !!! [MCU1_0] 27.984385 s: [1] Receive the heart from A53 core IPC! [C7x_1 ] 1.096164 s: CIO: Init ... Done !!! [C7x_1 ] 1.096184 s: APP: Init ... !!! [C7x_1 ] 1.096196 s: SCICLIENT: Init ... !!! [C7x_1 ] 1.096276 s: SCICLIENT: DMSC FW version [9.1.8--v09.01.08 (Kool Koala)] [C7x_1 ] 1.096295 s: SCICLIENT: DMSC FW revision 0x9 [C7x_1 ] 1.096310 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_1 ] 1.096325 s: SCICLIENT: Init ... Done !!! [C7x_1 ] 1.096337 s: UDMA: Init ... !!! [C7x_1 ] 1.096348 s: UDMA: Init ... Done !!! [C7x_1 ] 1.096374 s: MEM: Init ... !!! [C7x_1 ] 1.096387 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ b2000000 of size 117440512 bytes !!! [C7x_1 ] 1.096416 s: MEM: Init ... Done !!! [C7x_1 ] 1.096429 s: IPC: Init ... !!! [C7x_1 ] 1.096441 s: IPC: 3 CPUs participating in IPC !!! [C7x_1 ] 1.096665 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_1 ] 13.279430 s: IPC: HLOS is ready !!! [C7x_1 ] 13.279534 s: IPC: Init ... Done !!! [C7x_1 ] 13.279549 s: APP: Syncing with 2 CPUs ... !!! [C7x_1 ] 13.293334 s: APP: Syncing with 2 CPUs ... Done !!! [C7x_1 ] 13.293350 s: REMOTE_SERVICE: Init ... !!! [C7x_1 ] 13.294493 s: REMOTE_SERVICE: Init ... Done !!! [C7x_1 ] 13.294519 s: VX_ZONE_INIT:Enabled [C7x_1 ] 13.294534 s: VX_ZONE_ERROR:Enabled [C7x_1 ] 13.294548 s: VX_ZONE_WARNING:Enabled [C7x_1 ] 13.295278 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1 [C7x_1 ] 13.295391 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2 [C7x_1 ] 13.295495 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3 [C7x_1 ] 13.295597 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4 [C7x_1 ] 13.295698 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5 [C7x_1 ] 13.295799 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6 [C7x_1 ] 13.295901 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7 [C7x_1 ] 13.296003 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8 [C7x_1 ] 13.296029 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C7x_1 ] 13.296045 s: APP: OpenVX Target kernel init ... !!! [C7x_1 ] 13.296250 s: APP: OpenVX Target kernel init ... Done !!! [C7x_1 ] 13.296266 s: APP: Init ... Done !!! [C7x_1 ] 13.296280 s: APP: Run ... !!! [C7x_1 ] 13.296290 s: APP: Run ... Done !!! [MCU1_0] 30.026038 s: [2] Receive the heart from A53 core IPC! [MCU1_0] 32.017972 s: [3] Receive the heart from A53 core IPC! [MCU1_0] 34.017634 s: [4] Receive the heart from A53 core IPC! [MCU1_0] 36.017908 s: [5] Receive the heart from A53 core IPC! [MCU1_0] 38.018229 s: [6] Receive the heart from A53 core IPC! root@am62axx-evm:/usr/bin# root@am62axx-evm:/usr/bin# [I]Message: bagad client name is ebLogMgr [I]Start: pomp_ctx_new() success [I]client_start try to connect: client fd = 7 [I]client connect to server failed,res=-1,errno=115,reason=Operation now in progress [I]Start: pomp_ctx_connect() success, clinet fd is 7 [I]server_accept_conn: connection count is 2 bagad_server recv msg_id=00252166 [bagad server]: bind connection 2, process name: ebLogMgr bagad_server recv msg_id=00b95f3e notify_subscr: 1 009ae8f8 bagad_server recv msg_id=00b95f3e notify_subscr: 1 00fea229 [I]PompEvtCallback: register sharedinfo name: core_connect_status [I]PompEvtCallback: register sharedinfo name: SysLog bagad_server recv msg_id=00187a83 [I]PompEvtCallback: register sharedinfo name: diag_startup_notice bagad_server recv msg_id=00187a83 bagad_server recv msg_id=00187a83 bagad_server recv msg_id=009ae8f8 bagad_server recv msg_id=009ae8f8 [MCU1_0] 38.380932 s: LINUX_SEND_LOG_LEVEL: 6 bagad_server recv msg_id=009ae8f8 [MCU1_0] 40.017566 s: [7] Receive the heart from A53 core IPC! bagad_server recv msg_id=009ae8f8 [MCU1_0] 42.018301 s: [8] Receive the heart from A53 core IPC! bagad_server recv msg_id=009ae8f8 [MCU1_0] 44.018420 s: [9] Receive the heart from A53 core IPC! bagad_server recv msg_id=009ae8f8 [MCU1_0] 46.018315 s: [10] Receive the heart from A53 core IPC! [MCU1_0] 48.018142 s: [11] Receive the heart from A53 core IPC! bagad_server recv msg_id=009ae8f8 bagad_server recv msg_id=009ae8f8 [MCU1_0] 50.018181 s: [12] Receive the heart from A53 core IPC! bagad_server recv msg_id=009ae8f8 [MCU1_0] 52.017547 s: [13] Receive the heart from A53 core IPC! bagad_server recv msg_id=009ae8f8 [MCU1_0] 54.018054 s: [14] Receive the heart from A53 core IPC!
I try to set priority of appMain task to 8. but app_init() also can't be run complete.
It also stop in the step to initialize remote service.
[MCU1_0] 13.293576 s: REMOTE_SERVICE: Init ... !!!
Can you help us to analyze it together?
Thanks!
Best Regards,
Songqing Lin