Part Number: CCSTUDIO
Hello everyone,
I am trying to connect the BH-USB560V2 JTAG to the CCStudio on a guest Linux.
Thanks,
Tamas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CCSTUDIO
Hello everyone,
I am trying to connect the BH-USB560V2 JTAG to the CCStudio on a guest Linux.
Thanks,
Tamas
Hello,
I am trying to connect the BH-USB560V2 JTAG to the CCStudio on a guest Linux.
Can your provide more details? Are you trying to use CCS inside a Linux VM running on a Windows host? If so, what Linux distro and version are you running on the VM? What exact CCS version? Did you run the required CCS post-install drivers script to set the permissions on the drivers? What errors are you seeing?
Thanks
ki
Hy,
Are you trying to use CCS inside a Linux VM running on a Windows host? - Yes
What exact CCS version? - 12.6.0.00008
Did you run the required CCS post-install drivers script to set the permissions on the drivers? - Yes I do
What errors are you seeing? - When I set up the target configuration I am trying to test the connection. The ERROR code: E_RPCENV_IO_ERROR(-6) No connection: open failed: code 19
Using the lsusb I am seeing the JTAG: Bus 001 Device 003: ID 0b1e:0009 Electronic Warfare Assoc., Inc. (EWA) Blackhawk USB560v2 System Trace Emulator
Regards,
Tamas
The ERROR code: E_RPCENV_IO_ERROR(-6) No connection: open failed: code 19
This is a common host connection error (the CCS debugger is unable to communicate with the debug probe). The reasons can vary from a defective debug probe, issue with the host OS not detecting the probe, OS does not have permissions to access the debug probe (typically happens on Linux if the install_drivers.sh script is not run with sudo after CCS installation).
Assuming you DID run install_drivers.sh with sudo after CCS installation, AND the Linux guest is properly detecting the debug probe. Check to see if the debug probe is fully functional. Both USB and MODE LEDs should be SOLID GREEN when fully booted up and enumerated. See if everything works fine on the native Windows host.
Ubuntu 22.10 (Kinetic Kudu) 64-bit
Please note that we only officially support current Ubuntu LTS releases. 22.04LTS is the last officially supported one by CCS. I confirmed that I have no issues with my Blackhawk XDS560v2 running on my Ubuntu 22.04 LTS VM: