Other Parts Discussed in Thread: AM68, AM68A
I've got an HP Z23n G2 23-inch display connected via DisplayPort to my SK-AM68 dev board. I'm noticing that about ~25% of the time after rebooting the board, the coloring is incorrect.
This is what I expect:
This is what sometimes comes up:
Sometimes a simple reboot clears it up. Other times, it takes a few reboots to clear up. I'm not doing anything apart from issue "reboot" via the debug console. No other interaction is going on.
Any ideas what is causing this?
The SD card is programmed with the 'wic' image from here: https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-AM68A The page references this version info: "09.01.00.06 (08 Dec 2023)" and the m5dum checksum of my download matches what is reflected on that same page: 41296714ff0ce85c6e4b362f24146e5e