This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: QNX BSP Ethernet interface issues

Part Number: SK-AM62A-LP

Hey TI-experts,

We're having issues getting the ethernet interfaces running with the QNX BSP with the `ti-processor-sdk-qnx-am62axx_09_01_00_01` version.

Specifically using: `710_SVN977709_JBN6_am62a`.

(We've also tried the exact same with ti-processor-sdk-qnx-am62axx_09_00_00_01).

After booting the built SD card we're getting:


(Not containing an interface corresponding to the actual ethernet port).

Looking through the slog2info we can see some issues such as:

  • link_elf_load_file: devs-libpci.so load fail cause:Library cannot be found
  • Failed to open devs-libpci.so and ignore_pci not set
  • Error: ti_sci_msg_xfer (268): sciclient service call failed on ACK


We've tried making various changes to the recipe, but to no avail.

For instance relating to the network:

  • Involving `io-pkt-v6-hc` which we've used for other targets (building QNX for tda4al).
    • (However with this we're running into "ifconfig: getifaddrs: Bad message" outputs -- without any indication about what is actually missing).
  • Explicitly added the `cpsw2g` interface.
  • Various configurations for io-sock as outlined  here: www.qnx.com/.../index.html



Note that the below files are the outcome of using the SDK as-is building the QNX BSP following the instructions in the docs.

(Had to append .txt to get the post to accept it):

###################################################################################
#
# Neutrino 7.1 on TI AM62A EVM -  Added & Updated by TI
#
###################################################################################
[-optional]
[+keeplinked]
[image=0x80080000]
[virtual=aarch64le,raw +compress] .bootstrap = {
    #[+keeplinked] startup-am62a-evm -v
    #######################################################################
    # startup options:
    # [1] Carveout memory for remote cores (Added by TI).
    #  Start address is at 0x99A00000 and a total size is 0x26600000 (End address 0xBFFFFFFF).
    #    -r0x99A00000,0x26600000,1
    #  For Codec: HighMem region is default and carveout at 0x880000000, total size - 0x30000000
    #             Lowmem region can used for codec starting at : 0xC0000000, total size: 0x30000000 
    #######################################################################
    [+keeplinked] startup-am62a-evm -v -r0x99A00000,0x26600000,1 -r0xC0000000,0x30000000,1 ,-r0x880000000,0x30000000,1
    PATH=/proc/boot:/bin:/usr/bin:/sbin:/usr/sbin:/usr/lib
    LD_LIBRARY_PATH=/proc/boot:/lib:/usr/lib:/lib/dll:/lib/dll/pci procnto-smp-instr -v
}
[+script] .script = {
    # Programs require the runtime linker (ldqnx-64.so) to be at a fixed location
    procmgr_symlink ../../proc/boot/ldqnx-64.so.2 /usr/lib/ldqnx-64.so.2
    
    display_msg Welcome to QNX Neutrino 7.1.0 on the TI AM62A SK EVM Board!!
    ## Needed for ksh to run the echo command below
    pipe

    slogger2
    dumper -d /tmp
    mqueue
    random -p -t

    ############################################################################################
    ## I2C driver
    ############################################################################################
    display_msg "Starting I2C driver ..."
    i2c-omap35xx -p0x20000000 -i193 -d
    i2c-omap35xx -p0x20010000 -i194 -d --u1
    i2c-omap35xx -p0x20020000 -i195 -d --u2

    waitfor /dev/i2c0
    waitfor /dev/i2c1
    waitfor /dev/i2c2

    #######################################################################
    ## UART drivers
    #######################################################################
    display_msg "start serial driver"
    devc-seromap -e -F 0x02800000,210
    waitfor /dev/ser1

    ############################################################################################
    ## SD memory card / eMMC driver
    ############################################################################################
    #display_msg Starting MMC/SD memory card driver... eMMC
    #devb-sdmmc-am65x sdio addr=0x0fa10000,irq=165,timing=~hs400,timing=~hs200,emmc,bs=sscfg=0x8000 disk name=emmc

    display_msg Starting MMC/SD memory card driver... SD
    devb-sdmmc-am65x sdio addr=0x0fa00000,irq=115,bs=sscfg=0x8000:ldo=0x600000^31:trm-icp=2 cam pnp disk name=sd

    #######################################################################
    ## OSPI NAND ETFS spiflash driver using DAC controller without UDMA support and no DTR
    #######################################################################
    display_msg "Starting ETFS Flash OSPI driver..."
    fs-etfs-j7ospi-am62a-sk -Drclk=120000000,clk=60000000,rdelay=3r,dac=1,verbose=1 -r65536

    #######################################################################
    ## XHCI on both USB-C and A ports
    #######################################################################
    display_msg Starting XHCI driver on USB3SS0 and USB3SS1
    io-usb-otg -d dwc3-xhci ioport=0x31000000,irq=220,ioport=0x31100000,irq=258
    waitfor /dev/usb/io-usb-otg 10

    ############################################################################################
    ## CPSW3G Configuration
    ############################################################################################
    ## De-assert GPIO_CPSW1_RST(P01) to set as output
    sh -c "isend -n/dev/i2c1 -a0x22 0x0c > /dev/null 2>&1"
    sh -c "isendrecv -n /dev/i2c1 -a0x22 -l1 > /dev/null 2>&1"
    ## Returns ffh
    sh -c "isend -n/dev/i2c1 -a0x22 0x0c 0xfd > /dev/null 2>&1"
    sh -c "isend -n/dev/i2c1 -a0x22 0x0c > /dev/null 2>&1"
    sh -c "isendrecv -n /dev/i2c1 -a0x22 -l1 > /dev/null 2>&1"

    ## Set P01 to 1
    sh -c "isend -n/dev/i2c1 -a0x22 0x04 > /dev/null 2>&1"
    sh -c "isendrecv -n /dev/i2c1 -a0x22 -l1 > /dev/null 2>&1"
    # Returns ffh
    sh -c "isend -n/dev/i2c1 -a0x22 0x04 0xff > /dev/null 2>&1"
    sh -c "isend -n/dev/i2c1 -a0x22 0x04 > /dev/null 2>&1"
    sh -c "isendrecv -n /dev/i2c1 -a0x22 -l1 > /dev/null 2>&1"


    ############################################################################################
    ## Network driver
    ############################################################################################
    display_msg "Starting Network driver..."
    io-sock    -d axe -d axge -d cdce -d smsc
    
    ifwatchd -A /etc/newif.sh -D /etc/down.sh -c /etc/up.sh -n /etc/down.sh   axe0 axge0 cdce0 smsc0
    
    # Ensure that TCP/IP am0 interface is available before the script continue
    # if_up -p axge0

    # Set IP address
    # dhclient -m -lf /dev/shmem/dhclient.leases -pf /dev/shmem/dhclient.pid -nw axge0

    # Set static IP if needed
    # ifconfig axge0 192.168.0.1

    ############################################################################################
    ## REMOTE_DEBUG: gdb or Momentics
    ##  - refer to the help documentation for the gdb, qconn and the IDE
    ##    for more information on remote debugging
    ##  - the commands shown require that NETWORK is enabled too
    ############################################################################################
    #devc-pty
    #qconn
    #inetd

    #ksh /proc/boot/startup.sh

    ############################################################################################
    ## Start the main shell
    ############################################################################################
    reopen /dev/ser1
    
    export PCI_DEBUG_MODULE=/lib/dll/pci/pci_debug2.so
    export PCI_SLOG_MODULE=/lib/dll/pci/pci_slog2.so
    export PCI_BKWD_COMPAT_MODULE=/lib/dll/pci/pci_bkwd_compat.so

    #display_msg "Starting shell ..."
    #[+session] ksh &
    ### <--- For ti - start
    [+session] ksh /proc/boot/.console_ti.sh &
    #### For ti - end --->
}

[search=../install/${PROCESSOR}:../install/${PROCESSOR}/io-sock:../install:${QNX_TARGET}/${PROCESSOR}/io-sock:${QNX_TARGET}/io-sock:${QNX_TARGET}/${PROCESSOR}:${QNX_TARGET}]

[uid=0 gid=0]

[type=link] /bin/sh=/bin/ksh
[type=link] /tmp=/dev/shmem
[type=link] /dev/console=/dev/ser1
[type=link] /var/log=/tmp
[type=link] /usr/tmp=/tmp

################################################################################################
## Serial drivers
################################################################################################
/sbin/devc-seromap=sbin/devc-seromap

################################################################################################
## NAND etfs driver files
################################################################################################
/sbin/fs-etfs-j7ospi-am62a-sk=sbin/fs-etfs-j7ospi-am62a-sk

/usr/bin/etfsctl=usr/bin/etfsctl

###########################################################################
# fs-etfs-j7ospi-am62a support program
###########################################################################
/bin/etfs-magic=bin/etfs-magic

################################################################################################
## Block drivers
################################################################################################
/sbin/devb-ram=sbin/devb-ram
/sbin/devb-sdmmc-am65x=sbin/devb-sdmmc-am65x

################################################################################################
## Block driver support libraries
################################################################################################
/lib/libcam.so=lib/libcam.so
/lib/dll/io-blk.so=lib/dll/io-blk.so
/lib/dll/cam-disk.so=lib/dll/cam-disk.so
/lib/dll/cam-cdrom.so=lib/dll/cam-cdrom.so
/lib/dll/fs-qnx6.so=lib/dll/fs-qnx6.so
/lib/dll/fs-dos.so=lib/dll/fs-dos.so

################################################################################################
## Filesystems support
################################################################################################
/sbin/fdisk=sbin/fdisk
/sbin/mkdosfs=sbin/mkdosfs
/sbin/mkqnx6fs=sbin/mkqnx6fs
/sbin/chkdosfs=sbin/chkdosfs
/sbin/chkqnx6fs=sbin/chkqnx6fs

################################################################################################
## Network driver files
################################################################################################

/lib/dll/devs-axe.so=lib/dll/devs-axe.so
/lib/dll/devs-axge.so=lib/dll/devs-axge.so
/lib/dll/devs-cdce.so=lib/dll/devs-cdce.so
/lib/dll/devs-smsc.so=lib/dll/devs-smsc.so

################################################################################################
## Network driver shared libraries
################################################################################################
/usr/lib/libedit.so=usr/lib/libedit.so
/usr/lib/libexpat.so=usr/lib/libexpat.so
/usr/lib/libfdt.so=usr/lib/libfdt.so
/usr/lib/libxo.so.0=usr/lib/libxo.so.0

/lib/libsocket.so=lib/libsocket.so

/lib/dll/devs-libfdt.so=lib/dll/devs-libfdt.so
/lib/dll/devs-libpci.so=lib/dll/devs-libpci.so
/lib/dll/devs-libusbdci.so=lib/dll/devs-libusbdci.so
/lib/dll/devs-phy.so=lib/dll/devs-phy.so

/usr/lib/librpc.so=usr/lib/librpc.so

################################################################################################
## Network driver and support
################################################################################################
/sbin/dhclient=sbin/dhclient
[uid=0 gid=0 perms=0755] /sbin/dhclient-script=sbin/dhclient-script
/sbin/ifconfig=sbin/ifconfig
/sbin/io-sock=sbin/io-sock
/sbin/pfctl=sbin/pfctl
[uid=0 gid=0 perms=4755] /sbin/ping=sbin/ping
/sbin/route=sbin/route
/sbin/sysctl=sbin/sysctl

/usr/bin/ftp=usr/bin/ftp
/usr/bin/netstat=usr/bin/netstat
/usr/bin/sockstat=usr/bin/sockstat
/usr/bin/vmstat=usr/bin/vmstat

/usr/sbin/arp=usr/sbin/arp
/usr/sbin/devctl=usr/sbin/devctl
/usr/sbin/devinfo=usr/sbin/devinfo
/usr/sbin/fs-nfs3=usr/sbin/fs-nfs3
/usr/sbin/if_up=usr/sbin/if_up
/usr/sbin/ifmcstat=usr/sbin/ifmcstat
/usr/sbin/ifwatchd=usr/sbin/ifwatchd
/usr/sbin/ip6addrctl=usr/sbin/ip6addrctl
/usr/sbin/ndp=usr/sbin/ndp
/usr/sbin/rtsold=usr/sbin/rtsold
/usr/sbin/tcpdump=usr/sbin/tcpdump
[uid=0 gid=0 perms=4755] /usr/sbin/traceroute=usr/sbin/traceroute
[uid=0 gid=0 perms=4755] /usr/sbin/traceroute6=usr/sbin/traceroute6

/etc/dhclient.conf=etc/dhclient.conf
/etc/ftpusers=etc/ftpusers
/etc/hosts=etc/hosts
/etc/netconfig=etc/netconfig
/etc/protocols=etc/protocols
/etc/services=etc/services

################################################################################################
## Remote_debug
################################################################################################
/sbin/devc-pty=sbin/devc-pty
/usr/bin/pdebug=usr/bin/pdebug
/usr/sbin/qconn=usr/sbin/qconn

################################################################################################
## Network services (ssh) support
################################################################################################
[uid=0 gid=0 perms=0755] /usr/sbin/sshd=usr/sbin/sshd

[uid=0 gid=0 perms=0755] /usr/libexec/sftp-server=usr/libexec/sftp-server
[uid=0 gid=0 perms=0755] /usr/bin/scp=usr/bin/scp
[uid=0 gid=0 perms=0755] /usr/bin/ssh=usr/bin/ssh
[uid=0 gid=0 perms=0755] /usr/bin/ssh-keygen=usr/bin/ssh-keygen

################################################################################################
## Network services (telnet) support
################################################################################################
[uid=0 gid=0 perms=0755] /usr/sbin/inetd=usr/sbin/inetd
[uid=0 gid=0 perms=0755] /usr/libexec/ftpd=usr/libexec/ftpd
[uid=0 gid=0 perms=0755] /usr/libexec/telnetd=usr/libexec/telnetd

[uid=0 gid=0 perms=0755]/etc/newif.sh = {
#!/bin/sh
ifconfig $1 up
}

[uid=0 gid=0 perms=0755]/etc/up.sh = {
#!/bin/sh
dhclient -m -lf /dev/shmem/dhclient.leases.$1 -pf /dev/shmem/dhclient.pid.$1 -nw $1
}

[uid=0 gid=0 perms=0755]/etc/down.sh = {
#!/bin/sh
dhclient -m -lf /dev/shmem/dhclient.leases.$1 -pf /dev/shmem/dhclient.pid.$1 -x $1
}

## NOTE: The following is very insecure and must not be used in a production
##       environment.  This allows telnet access to root without a password!
##       Even with a password this is not secure as telnet passes the password
##       unencrypted over the network.  NO NOT USE THIS IN AN UNSECURED ENVIRONMENT!
##       This configuration is only meant for initial setup and testing of a new board.
##       If you need network access use a secure protocol like ssh (e.g. OpenSSH or Drop Bear).
##
/etc/inetd.conf = {
telnet stream tcp nowait root /usr/libexec/telnetd in.telnetd
ftp stream tcp nowait root /usr/libexec/ftpd in.ftpd -l
}

/etc/ftpd.conf = {
/* Make things a+rw by default */
umask all 0000
}

/etc/esh = {
}

################################################################################################
## USB HOST drivers
################################################################################################
/lib/dll/devu-hcd-dwc3-xhci.so=lib/dll/devu-hcd-dwc3-xhci.so

################################################################################################
## USB host shared libraries
################################################################################################
/lib/libhiddi.so=lib/libhiddi.so
/lib/libusbdi.so=lib/libusbdi.so

################################################################################################
## USB host driver and support
################################################################################################
/sbin/io-usb-otg=sbin/io-usb-otg
/sbin/usb=sbin/usb
/sbin/devb-umass=sbin/devb-umass

################################################################################################
## USB device shared libraries
################################################################################################
/lib/libusbdci.so=lib/libusbdci.so

################################################################################################
## I2C drivers
################################################################################################
/sbin/i2c-omap35xx=sbin/i2c-omap35xx

################################################################################################
## I2C support
################################################################################################
/bin/isendrecv=bin/isendrecv
/bin/isend=bin/isend

################################################################################################
## Shared libraries for security
################################################################################################
/lib/libqh.so=lib/libqh.so
/lib/libregex.so=lib/libregex.so
/lib/libsecpol.so=lib/libsecpol.so
/lib/libslog2parse.so=lib/libslog2parse.so
/lib/libslog2shim.so=lib/libslog2shim.so
/lib/libslog2.so=lib/libslog2.so
/lib/libtracelog.so=lib/libtracelog.so

/lib/dll/qcrypto-openssl.so=lib/dll/qcrypto-openssl.so

/usr/lib/libcrypto.so=usr/lib/libcrypto.so
/usr/lib/libncursesw.so=usr/lib/libncursesw.so
/usr/lib/libqcrypto.so=usr/lib/libqcrypto.so
/usr/lib/libssl.so=usr/lib/libssl.so

################################################################################################
## libqcrypto support
################################################################################################
[uid=0 gid=0 perms=0644] /etc/qcrypto.conf = {
openssl     tags=*
}

################################################################################################
## Security files
################################################################################################
[uid=0 gid=0 perms=4755] /bin/login=bin/login
[uid=0 gid=0 perms=4755] /bin/su=bin/su
[uid=0 gid=0 perms=4755] /usr/bin/passwd=usr/bin/passwd

[uid=0 gid=0 perms=0644] /etc/passwd = {
root:x:0:0:Superuser:/root:/bin/sh
sshd:x:15:6:sshd:/var/chroot/sshd:/bin/false
qnxuser:x:1000:1000:QNX User:/home/qnxuser:/bin/sh
}

## Enabled Username/Password: root/root, qnxuser/qnxuser
[uid=0 gid=0 perms=0644] /etc/shadow = {
root:@S@NKlWES1quMp1wmqugkUSnFEpPGn58kIs4wQOgDDNs06vimR+bbGPUKM+9P6jbFUzo3Rm+Qe5MS+17xKhwaeJEg==@Mjg5ZTJiMTM0YTRjYTE2ZGFjMDdhZTFlY2NlMDVmNmE=:1468494669:0:0
sshd:*:1231323780:0:0
qnxuser:@S@HZERXjgixvb3157FFeraShhvTVw+10ccUtVUVZbi0fUwpzlzBZFw5gHiFd1XHKit8D39Whe749XAY8fV4P5ANQ==@Y2ZlOTg3M2RhNTM4Y2M2ODY0OWZhODdiNDRkMmU5Nzg=:1468488235:0:0
}

[uid=0 gid=0 perms=0644] /etc/group = {
root:x:0:root
sshd:x:6:
qnxuser:x:1000
}

################################################################################################
## PAM configurations addon build file
################################################################################################
[uid=0 gid=0 type=dir dperms=0755] /
[uid=0 gid=0 type=dir dperms=0755] /etc
[uid=0 gid=0 type=dir dperms=0755] /etc/pam.d
[uid=0 gid=0 type=dir dperms=0755] /home
[uid=1000 gid=1000 type=dir dperms=0755] /home/qnxuser
[uid=0 gid=0 type=dir dperms=0755] /lib
[uid=0 gid=0 type=dir dperms=0700] /root
[uid=0 gid=0 type=dir dperms=0755] /usr
[uid=0 gid=0 type=dir dperms=0755] /usr/lib
[uid=0 gid=0 type=dir dperms=0755] /var
[uid=0 gid=0 type=dir dperms=0755] /var/chroot
[uid=0 gid=0 type=dir dperms=0755] /var/chroot/sshd
[uid=0 gid=0 type=dir dperms=0755] /var/db
[uid=0 gid=0 type=dir dperms=0755] /var/run

[uid=0 gid=0 perms=0644] /etc/pam.d/ftpd=etc/pam.d/ftpd
[uid=0 gid=0 perms=0644] /etc/pam.d/login=etc/pam.d/login
[uid=0 gid=0 perms=0644] /etc/pam.d/passwd=etc/pam.d/passwd
[uid=0 gid=0 perms=0644] /etc/pam.d/su=etc/pam.d/su

[uid=0 gid=0 perms=0755] /usr/lib/libpam.so=usr/lib/libpam.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_deny.so=usr/lib/pam_deny.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_echo.so=usr/lib/pam_echo.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_exec.so=usr/lib/pam_exec.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_ftpusers.so=usr/lib/pam_ftpusers.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_group.so=usr/lib/pam_group.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_mac.so=usr/lib/pam_mac.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_permit.so=usr/lib/pam_permit.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_qnx.so=usr/lib/pam_qnx.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_rootok.so=usr/lib/pam_rootok.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_secpol.so=usr/lib/pam_secpol.so
[uid=0 gid=0 perms=0755] /usr/lib/pam_self.so=usr/lib/pam_self.so

################################################################################################
## General shared libraries
################################################################################################
ldqnx-64.so.2=usr/lib/ldqnx-64.so.2

/lib/libc.so=lib/libc.so
/lib/libcatalog.so=lib/libcatalog.so
/lib/libdevice-publisher.so=lib/libdevice-publisher.so
/lib/libgcc_s.so=lib/libgcc_s.so
/lib/libm.so=lib/libm.so
/lib/libpps.so=lib/libpps.so

/usr/lib/libbacktrace.so=usr/lib/libbacktrace.so
/usr/lib/libc++.so=usr/lib/libc++.so
/usr/lib/libiconv.so=usr/lib/libiconv.so
/usr/lib/libintl.so=usr/lib/libintl.so
/usr/lib/libpanelw.so=usr/lib/libpanelw.so
/usr/lib/libz.so=usr/lib/libz.so

################################################################################################
## General commands
################################################################################################
/bin/cat=bin/cat
/bin/chmod=bin/chmod
/bin/confstr=bin/confstr
/bin/cp=bin/cp
/bin/dd=bin/dd
/bin/df=bin/df
/bin/echo=bin/echo
/bin/hostname=bin/hostname
/bin/kill=bin/kill
/bin/ksh=bin/ksh
/bin/ln=bin/ln
/bin/ls=bin/ls
/bin/mkdir=bin/mkdir
/bin/mount=bin/mount
/bin/mv=bin/mv
/bin/on=bin/on
/bin/pidin=bin/pidin
/bin/pwd=bin/pwd
/bin/rm=bin/rm
/bin/sed=bin/sed
/bin/slay=bin/slay
/bin/slog2info=bin/slog2info
/bin/slogger2=bin/slogger2
/bin/sync=bin/sync
/bin/umount=bin/umount
/bin/uname=bin/uname
/bin/waitfor=bin/waitfor

/sbin/mqueue=sbin/mqueue
/sbin/pipe=sbin/pipe
/sbin/shutdown=sbin/shutdown

/usr/bin/date=usr/bin/date
/usr/bin/env=usr/bin/env
/usr/bin/find=usr/bin/find
/usr/bin/grep=usr/bin/grep
/usr/bin/getconf=usr/bin/getconf
/usr/bin/hd=usr/bin/hd
/usr/bin/ldd=usr/bin/ldd
/usr/bin/more=usr/bin/more
/usr/bin/setconf=usr/bin/setconf
/usr/bin/sleep=usr/bin/sleep
/usr/bin/tty=usr/bin/tty
/usr/bin/top=usr/bin/top
/usr/bin/use=usr/bin/use
/usr/bin/which=usr/bin/which

/usr/sbin/dumper=usr/sbin/dumper
/usr/sbin/random=usr/sbin/random
/usr/sbin/tracelogger=usr/sbin/tracelogger

################################################################################################
## startup script
################################################################################################
[perms=0700] startup.sh = {
    if [ -e /dev/sd0t179 ]; then
        echo "Mounting QNX filesystem sd0t179 to /mnt"
        mount -t qnx6 /dev/sd0t179 /mnt
        waitfor /mnt

    elif [ -e /dev/emmc0t179 ]; then
        echo "Mounting QNX filesystem emmc0t179 to /mnt"
        mount -t qnx6 /dev/emmc0t179 /mnt
        waitfor /mnt

    fi

    if [ -e /mnt/scripts/startup.sh  ]; then
        echo "Running system startup script"
        ksh /mnt/scripts/startup.sh
    fi
}

/lib/libpci.so=lib/libpci.so

### <--- For ti -start
###########################################################################
## Set environment and start the main shell
###########################################################################
[perms=0744] .console_ti.sh={

        # These environment variables are inherited by all the programs that follow.
        echo Setting environment variables...
        export SYSNAME=nto
        export TERM=qansi
        export HOME=/
        export PS1="AM62AEVM# "
        export PATH=/proc/boot:/bin:/usr/bin:/sbin:/usr/sbin:/usr/lib
        export LD_LIBRARY_PATH=/proc/boot:/lib:/usr/lib:/lib/dll:/lib/dll/pci

        #######################################################################
        ## Run user script if it exists
        #######################################################################
        echo Mounting the sd ..
        waitfor /dev/sd0 10
        mount -tdos -oexe=all /dev/sd0t12 /boot
        mount -tdos -oexe=all /dev/sd0t12.1 /ti_fs
        echo Looking for user script to run: /ti_fs/scripts/user.sh
        waitfor /ti_fs/scripts/user.sh
        user_script=/ti_fs/scripts/user.sh
        if [ -e "$user_script" ]; then
                echo Running user script...
                . "$user_script"
        fi

        echo done...
        ksh -l
}

#### For ti - end --->

################################################################################################
## END OF BUILD SCRIPT
################################################################################################




And the corresponding slog2info:
AM62A-EVM@QNX:/# slog2info
Jan 01 00:00:00.046                       random.6                  low*     0  qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)]
Jan 01 00:00:00.047                    random.6..0                 slog*   700  Random is using the Fortuna PRNG
Jan 01 00:00:00.055                       random.6                  low      0  qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)]
Jan 01 00:00:00.055                    random.6..0                 slog    700  Selecting timer as an entropy source
Jan 01 00:00:00.055                    random.6..0                 slog    700  Using entropy from syspoll as an entropy source
Jan 01 00:00:00.055                    random.6..0                 slog    700  Registered path names
Jan 01 00:00:00.056                    random.6..0                 slog    700  random: all library entropy sources started
Jan 01 00:00:00.056                    random.6..0                 slog    700  random: starting resmgr
Jan 01 00:00:00.056                    random.6..0                 slog    700  random: Daemonizing the process
Jan 01 00:00:00.084            devb_sdmmc_am65x.11                 slog*  1800  devb-sdmmc-am65x 1.00A (Mar 25 2024 14:28:15)
Jan 01 00:00:00.085            devb_sdmmc_am65x.11                 slog      0  libcam.so (Sep  3 2021 11:57:38) bver 7010004
Jan 01 00:00:00.085            devb_sdmmc_am65x.11                 slog   1800  Detected: TI_AM62A_SK_EVM_Board
Jan 01 00:00:00.085            devb_sdmmc_am65x.11                 slog   1800  sdio_cd:  insertion path 0, cd state 0x1
Jan 01 00:00:00.099                io_usb_otg.4108                 slog*     0  main(453)[tid:1]: io-usb-otg (Jul 26 2021 16:07:38) args: -d dwc3-xhci ioport=0x31000000,irq=220,ioport=0x31100000,irq=258
Jan 01 00:00:00.105                io_usb_otg.4108                 slog      0  xhci_init: Initialiaing with sever version: 2
Jan 01 00:00:00.105                io_usb_otg.4108                 slog      0  xhci_controller_init(2729): devu-hcd-dwc3-xhci.so (May  9 2023 10:44:49):  args
Jan 01 00:00:00.105                io_usb_otg.4108                 slog      8  usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, Super speed
Jan 01 00:00:00.105                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 8)
Jan 01 00:00:00.106                io_usb_otg.4108                 slog     12  usb_device_set_address(245)[tid:1]: b:0 devno 0
Jan 01 00:00:00.106                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
Jan 01 00:00:00.106                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
Jan 01 00:00:00.106                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
Jan 01 00:00:00.107                io_usb_otg.4108                 slog      8  usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0)
Jan 01 00:00:00.107                io_usb_otg.4108                 slog     11  hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
Jan 01 00:00:00.107                io_usb_otg.4108                 slog     13  hub_configuration_enable(263)[tid:1]: 1
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800  SD CID:
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    MID 0x9f, OID 0x5449, PNM SDCHE
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    PRV 0xe8, PSN 0x7ce800d5, MDT 8-2022
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800  SD CSD:
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    TAAC 14, NSAC 0, TRAN_SPEED 50
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    C_SIZE 59743, C_SIZE_MULT 0
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    READ_BL_LEN 9, WRITE_BL_LEN 9
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    blksz 512, sectors 61177856, dtr 25000000
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800  SD SW CAPS:
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    bus mode 0x1f, cmd sys 0x1
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    drv type 0xf, curr limit 0xf
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800    dtr 50000000
Jan 01 00:00:00.140            devb_sdmmc_am65x.11                 slog   1800  CFG:  Timing SDR104, DTR 200000000, Bus Width 4 bit

Jan 01 00:00:00.141            devb_sdmmc_am65x.11                 slog    100  cam-disk.so (Sep  3 2021 11:57:42)
Jan 01 00:00:00.208                io_usb_otg.4108                 slog      0  xhci_init: Initialiaing with sever version: 2
Jan 01 00:00:00.208                io_usb_otg.4108                 slog      0  xhci_controller_init(2729): devu-hcd-dwc3-xhci.so (May  9 2023 10:44:49):  args
Jan 01 00:00:00.208                io_usb_otg.4108                 slog      8  usb_enum_port(94)[tid:1]: busno 1, parent -1, port 0, Super speed
Jan 01 00:00:00.209                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 8)
Jan 01 00:00:00.209                io_usb_otg.4108                 slog     12  usb_device_set_address(245)[tid:1]: b:1 devno 0
Jan 01 00:00:00.209                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
Jan 01 00:00:00.209                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
Jan 01 00:00:00.209                io_usb_otg.4108                 slog     11  usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
Jan 01 00:00:00.210                io_usb_otg.4108                 slog      8  usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 1, devno 0:1)
Jan 01 00:00:00.210                io_usb_otg.4108                 slog     11  hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0
Jan 01 00:00:00.210                io_usb_otg.4108                 slog     13  hub_configuration_enable(263)[tid:1]: 1
Jan 01 00:00:00.312                io_usb_otg.4108                 slog      0  usbh_timeout_init(203)[tid:1]: Complete
Jan 01 00:00:00.404              io_sock.126989..0          main_buffer*     1  io-sock -d axe -d axge -d cdce -d smsc
Jan 01 00:00:00.408              io_sock.126989..0          main_buffer      1  Copyright (c) 1992-2021 The FreeBSD Project.
Jan 01 00:00:00.408              io_sock.126989..0          main_buffer      1  Copyright (c) 1979, 1980, 1983, 1986, 1988, 1989, 1991, 1992, 1993, 1994
Jan 01 00:00:00.408              io_sock.126989..0          main_buffer      1          The Regents of the University of California. All rights reserved.
Jan 01 00:00:00.408              io_sock.126989..0          main_buffer      1  FreeBSD is a registered trademark of The FreeBSD Foundation.
Jan 01 00:00:00.408              io_sock.126989..0          main_buffer      1  FreeBSD 13.0-RELEASE-p11 #0: Wed May 10 12:25:54 EDT 2023
Jan 01 00:00:00.408              io_sock.126989..0          main_buffer      1      builder@sdp710-node1:/builds/workspace/710-SDP/build_aarch64/lib/io-sock/sys/target/aarch64-o.le
Jan 01 00:00:00.408              io_sock.126989..0          main_buffer      1  ntoaarch64-gcc (QNX7.1.0-r1659-58) 8.3.0
Jan 01 00:00:00.424              io_sock.126989..0          main_buffer      1  Driver fullpath: /lib/dll/devs-phy.so
Jan 01 00:00:00.425              io_sock.126989..0          main_buffer      1  wlan: mac acl policy registered
Jan 01 00:00:00.428              io_sock.126989..0          main_buffer      1  link_elf_load_file: devs-libpci.so load fail cause:Library cannot be found
Jan 01 00:00:00.428              io_sock.126989..0          main_buffer      1  Failed to open devs-libpci.so and ignore_pci not set
Jan 01 00:00:00.429              io_sock.126989..0          main_buffer      1  Driver fullpath: /lib/dll/devs-libusbdci.so
Jan 01 00:00:00.429              io_sock.126989..0          main_buffer      1  cryptosoft0: <software crypto> on QNX
Jan 01 00:00:00.430              io_sock.126989..0          main_buffer      1  iousb0: <io-usb-otg> on QNX
Jan 01 00:00:00.430              io_sock.126989..0          main_buffer      1  iousb0: Connecting to default usb stack (NULL)
Jan 01 00:00:00.430                io_usb_otg.4108                 slog      0  usbdi_client_connect(58)[tid:5]: pid 126989 proc=sbin/io-sock usbdi_client 4061c51230
Jan 01 00:00:00.430                io_usb_otg.4108                 slog      0  usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 126989 usbdi_client 4061c51230
Jan 01 00:00:00.431              io_sock.126989..0          main_buffer      1  iousb0: Initialize bus:0.  XHCI controller_type:1 state:1 ndev:0
Jan 01 00:00:00.431              io_sock.126989..0          main_buffer      1  uhub0: <QNX USB controller> on iousb0
Jan 01 00:00:00.431              io_sock.126989..0          main_buffer      1  iousb0: Initialize bus:1.  XHCI controller_type:1 state:0 ndev:0
Jan 01 00:00:00.431              io_sock.126989..0          main_buffer      1  uhub1: <QNX USB controller> on iousb0
Jan 01 00:00:00.431                io_usb_otg.4108                 slog      0  usbdi_client_connect(58)[tid:5]: pid 126989 proc=sbin/io-sock usbdi_client 4061c4e610
Jan 01 00:00:00.432              io_sock.126989..0          main_buffer      1  Event timer "QNX" frequency 1000 Hz quality 600
Jan 01 00:00:00.432              io_sock.126989..0          main_buffer      1  Timecounters tick every 1.000 msec
Jan 01 00:00:00.432              io_sock.126989..0          main_buffer      1  Timecounter "QNX" frequency 200000000 Hz quality 600
Jan 01 00:00:00.432              io_sock.126989..0          main_buffer      1  [fib_algo] fib_module_register: attaching dpdk_lpm6 to inet6
Jan 01 00:00:00.432              io_sock.126989..0          main_buffer      1  [fib_algo] fib_module_register: attaching dpdk_lpm4 to inet
Jan 01 00:00:00.432                io_usb_otg.4108                 slog      0  usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 126989 usbdi_client 4061c4e610
Jan 01 00:00:00.437              io_sock.126989..0          main_buffer      1  [fib_algo] fib_module_register: attaching radix6_lockless to inet6
Jan 01 00:00:00.437              io_sock.126989..0          main_buffer      1  [fib_algo] fib_module_register: attaching radix6 to inet6
Jan 01 00:00:00.437              io_sock.126989..0          main_buffer      1  [fib_algo] fib_module_register: attaching bsearch4 to inet
Jan 01 00:00:00.437              io_sock.126989..0          main_buffer      1  [fib_algo] fib_module_register: attaching radix4_lockless to inet
Jan 01 00:00:00.437              io_sock.126989..0          main_buffer      1  [fib_algo] fib_module_register: attaching radix4 to inet
Jan 01 00:00:00.480              io_sock.126989..0          main_buffer     10  lo0: link state changed to UP
Jan 01 00:00:00.481              io_sock.126989..0          main_buffer      1  io-sock startup complete
Jan 01 00:00:00.481              io_sock.126989..0          main_buffer     50  devs-axe.so: loading module with ""
Jan 01 00:00:00.482              io_sock.126989..0          main_buffer     50  Driver fullpath: /lib/dll/devs-axe.so
Jan 01 00:00:00.483              io_sock.126989..0          main_buffer     50  devs-axe.so: loaded
Jan 01 00:00:00.483              io_sock.126989..0          main_buffer     50  devs-axge.so: loading module with ""
Jan 01 00:00:00.483              io_sock.126989..0          main_buffer     50  Driver fullpath: /lib/dll/devs-axge.so
Jan 01 00:00:00.484              io_sock.126989..0          main_buffer     50  devs-axge.so: loaded
Jan 01 00:00:00.484              io_sock.126989..0          main_buffer     50  devs-cdce.so: loading module with ""
Jan 01 00:00:00.484              io_sock.126989..0          main_buffer     50  Driver fullpath: /lib/dll/devs-cdce.so
Jan 01 00:00:00.484              io_sock.126989..0          main_buffer     50  devs-cdce.so: loaded
Jan 01 00:00:00.485              io_sock.126989..0          main_buffer     50  devs-smsc.so: loading module with ""
Jan 01 00:00:00.485              io_sock.126989..0          main_buffer     50  Driver fullpath: /lib/dll/devs-smsc.so
Jan 01 00:00:00.485              io_sock.126989..0          main_buffer     50  devs-smsc.so: loaded
Jan 01 00:00:00.487                      console.3                  out*     0  [126990] Jan 01 00:00:00 ifwatchd[126990-1]: watching interface axe0
Jan 01 00:00:00.488                      console.3                  out      0  [126990] Jan 01 00:00:00 ifwatchd[126990-1]: watching interface axge0
Jan 01 00:00:00.488                      console.3                  out      0  [126990] Jan 01 00:00:00 ifwatchd[126990-1]: watching interface cdce0
Jan 01 00:00:00.489                      console.3                  out      0  [126990] Jan 01 00:00:00 ifwatchd[126990-1]: watching interface smsc0
Jan 01 00:00:00.519                io_usb_otg.4108                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 0, pdevno 0, portno 1)
Jan 01 00:00:00.519                io_usb_otg.4108                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
Jan 01 00:00:00.709               tisci_mgr.184334                 slog*    55  TISCI resmgr for SOC AM62A (version=, date=tor 28 mar 2024 21:51:12 CET)
Jan 01 00:00:00.709               tisci_mgr.184334                 slog     55   SYSFW Firmware Version 8.6.4--v08.06.04 (Chill Capybar
Jan 01 00:00:00.709               tisci_mgr.184334                 slog     55   SYSFW Firmware revision 0x8
Jan 01 00:00:00.709               tisci_mgr.184334                 slog     55   SYSFW ABI revision 3.1
Jan 01 00:00:00.721          shmemallocator.196625                 slog*     0  SharedMemoryAllocator: BaseAddress: 0xa3000000 Size: 0x0e000000 (234881024)

Jan 01 00:00:00.721          shmemallocator.196625                 slog      0  initSHM:Block[0] @ 0xa3000000 has free-mem = 0xe000000 - 224 M

Jan 01 00:00:00.721          shmemallocator.196625                 slog      0  SharedMemoryAllocator: BaseAddress: 0x880000000 Size: 0x30000000 (805306368)

Jan 01 00:00:00.721          shmemallocator.196625                 slog      0  initSHM:Block[1] @ 0x880000000 has free-mem = 0x30000000 - 768 M

Jan 01 00:00:00.726                io_usb_otg.4108                 slog      8  usb_enum_port_extract(172)[tid:8]: (busno 1, pdevno 0, portno 1)
Jan 01 00:00:00.726                io_usb_otg.4108                 slog      8  usb_enum_port_extract(192)[tid:8]: status (2)
Jan 01 00:00:00.739               tiipc_mgr.200722                 slog*    57  TI IPC resmgr for SOC AM62A (version=, date=tor 28 mar 2024 21:51:12 CET)
Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  tiipc-mgr: Starting TI IPC Resmgr
Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  tiipc-mgr: Using VRING base address: 0xa0000000, size:0x300000
Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  [IPC]
Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  Mailbox_plugInterrupt: interrupt Number 108, arg 0x17D43518

Jan 01 00:00:00.739               tiipc_mgr.200722                 slog      0  MAILBOX: Mailbox Driver (4517d43348) open successful.

Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  [IPC]
Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  Mailbox_plugInterrupt: interrupt Number 109, arg 0x17D43738

Jan 01 00:00:00.739               tiipc_mgr.200722                 slog      0  MAILBOX: Mailbox Driver (4517d433b8) open successful.

Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  [IPC]
Jan 01 00:00:00.739               tiipc_mgr.200722                 slog     57  Mailbox_plugInterrupt: interrupt Number 140, arg 0x17D43958

Jan 01 00:00:00.740               tiipc_mgr.200722                 slog      0  MAILBOX: Mailbox Driver (4517d43428) open successful.

Jan 01 00:00:00.759               tisci_mgr.184334                 slog     55  Error: ti_sci_msg_xfer (268): sciclient service call failed on ACK
Jan 01 00:00:00.760               tisci_mgr.184334                 slog     55  Error: ti_sci_msg_xfer (268): sciclient service call failed on ACK
Jan 01 00:00:00.765               tisci_mgr.184334                 slog     55  Error: ti_sci_msg_xfer (268): sciclient service call failed on ACK
Jan 01 00:00:00.786        ti_vpu_codec_mgr.208916                 slog*    99  Starting VPU Codec resource manager...

Jan 01 00:00:00.786        ti_vpu_codec_mgr.208916                 slog     99  Starting VPU core 0

Jan 01 00:00:00.786          shmemallocator.196625                 slog      0  alloc_shm: Request allocation for block ID 1, of length 0x10000000

Jan 01 00:00:00.811          shmemallocator.196625                 slog      0  alloc_shm:Block[1] @ 0x880000000 has free-mem = 0x20000000 - 512 M

Jan 01 00:00:00.811        ti_vpu_codec_mgr.208916                 slog     99  vdi_init core[0] - phys_addr = 0x880000000 size = 0x10000000
Jan 01 00:00:00.811        ti_vpu_codec_mgr.208916                 slog     99  [VDI] vdi_allocate_common_memory - core_idx - 0 physaddr=0x880000000, virtaddr=0x2d1b166000, size=0x300000(3145728)
Jan 01 00:00:00.813        ti_vpu_codec_mgr.208916                 slog     99  [VDI] successful driver init

Jan 01 00:00:00.813        ti_vpu_codec_mgr.208916                 slog     99  [VDI] invalid interrupt info referenced

Jan 01 00:00:00.813          shmemallocator.196625                 slog      0
free_shm: Freeing memory at block 1 of size  0x10000000

Jan 01 00:00:00.823          shmemallocator.196625                 slog      0  free_shm:Block[1] @ 0x880000000 has free-mem = 0x30000000 - 768 M

Jan 01 00:00:00.824        ti_vpu_codec_mgr.208916                 slog     99  tivpu_codec_init:42 product id: 2

Jan 01 00:00:00.846          shmemallocator.196625                 slog      0  alloc_shm: Request allocation for block ID 1, of length 0x10000000

Jan 01 00:00:00.871          shmemallocator.196625                 slog      0  alloc_shm:Block[1] @ 0x880000000 has free-mem = 0x20000000 - 512 M

Jan 01 00:00:00.871        ti_vpu_codec_mgr.208916                 slog     99  vdi_init core[0] - phys_addr = 0x880000000 size = 0x10000000
Jan 01 00:00:00.871        ti_vpu_codec_mgr.208916                 slog     99  [VDI] vdi_allocate_common_memory - core_idx - 0 physaddr=0x880000000, virtaddr=0x2d1b476000, size=0x300000(3145728)
Jan 01 00:00:00.872        ti_vpu_codec_mgr.208916                 slog     99  [VDI] successful driver init

Jan 01 00:00:00.872        ti_vpu_codec_mgr.208916                 slog     99  [VDI] vdi_get_common_memory physaddr=0x880000000, virtaddr=0x2d1b476000, size=0x300000(3145728)
Jan 01 00:00:00.872        ti_vpu_codec_mgr.208916                 slog     99  VPU INIT Start!!!

Jan 01 00:00:00.874        ti_vpu_codec_mgr.208916                 slog     99   VPU registered in polling mode
Jan 01 00:00:00.897                  screen.213013                 slog*   300  screen: starting up...
Jan 01 00:00:00.899                  screen.213013                 slog    300  screen: Configuration file:  /ti_fs/usr/lib/graphics/am62a/graphics.conf
Jan 01 00:00:00.911                  screen.213013                 slog    200  [j7_wfd]INFO: Defaulting to BT601 limited range for video1-cs
Jan 01 00:00:00.911                  screen.213013                 slog    200  [j7_wfd]INFO: Defaulting to BT601 limited range for videolite1-cs
Jan 01 00:00:00.912                  screen.213013                 slog    300  screen: slog2 context created with 1 pages
Jan 01 00:00:00.912                  screen.213013                 slog    300  screen: loading alloc module jacinto7-alloc...
Jan 01 00:00:00.915                  screen.213013                 slog    300  screen: loading libhiddi.so...
Jan 01 00:00:00.915                  screen.213013                 slog    300  screen: server is ready
Jan 01 00:00:00.917                  screen.213013                 slog    200  [wfdcfg] [TCA6424] HDMI transmitter reset completed.
Jan 01 00:00:00.917                  screen.213013                 slog    200  [wfdcfg] [SiI9022A] starting HDMI transmitter configuration.
Jan 01 00:00:01.080                  screen.213013                 slog    200  [wfdcfg] [SiI9022A] graphics mode 1920x1080@60 [htotal:2200, vtotal:1125, pclk:148500KHz]
Jan 01 00:00:01.082                  screen.213013                 slog    200  [wfdcfg] [SiI9022A] HDMI transmitter configuration finished.




Assistance in the matter would be greatly appreciated,
Thank you

Best regards,
Oskar


  • Hi Oskar,

    For AM62A, the ethernet and networking support is provided by Blackberry through the io-sock package available on QNX Software Center. Once this package is properly setup, you would able to view the cpsw interfaces as part of ifconfig.

    Can you please check with Blackberry on this issue ? In case you are missing some setup step or binaries, they will be able to assist you directly on this

    Regards,

    Shiva