Designed a board using the AM62x STARTER KIT EVM as a reference but currently not booting through SD card; using the same configuration as the evaluation board (note, we are able to boot via SD Card using the EVM). Using AM6254ATCGGAALW. The circuit is identical to the EVM only using resistors instead of switches. the Terminal is communicating via FT234XD-R in the board.