SK-AM62A-LP: 'cryptodev': Cannot allocate memory

Part Number: SK-AM62A-LP
Other Parts Discussed in Thread: SK-AM62, AM62A7,

Hello

We are currently using SDK 9.01 and applying Falcon Mode.

And to boot from emmc, I set bootargs as below.


bootargs = "console=ttyS2,115200 root=/dev/mmcblk0p1 rw rootfstype=ext4";

However, after booting, loading the kernel module fails.


The log is as follows. Is there a solution?


root@am62axx-evm:/opt/edgeai-gst-apps# systemctl status systemd-modules-load.service
x systemd-modules-load.service - Load Kernel Modules
     Loaded: loaded (/lib/systemd/system/systemd-modules-load.service; static)
     Active: failed (Result: exit-code) since Thu 2022-04-28 18:20:43 UTC; 29s ago
       Docs: man:systemd-modules-load.service(8)
             man:modules-load.d(5)
    Process: 171 ExecStart=/lib/systemd/systemd-modules-load (code=exited, status=1/FAILURE)
   Main PID: 171 (code=exited, status=1/FAILURE)

Apr 28 18:20:43 am62axx-evm systemd-modules-load[171]: Failed to insert module 'cryptodev': Cannot allocate memory
Apr 28 18:20:43 am62axx-evm systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE
Apr 28 18:20:43 am62axx-evm systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'.
Apr 28 18:20:43 am62axx-evm systemd[1]: Failed to start Load Kernel Modules.
Notice: journal has been rotated since unit was started, output may be incomplete.