Hello,
I am working with OMAP3EVM (DM3730) development board. I need to use mouse over USB OTG port available with board instead of standard USB port.
I have done the following configuration in the kernel:
Device Drivers--> USB Support --> Driver Mode (Both host and peripheral...)
I also tried by sorting the pin 4 and 5 of OTG as suggested at the BeagleBoard Support Web Page.
But my board is not detecting the mouse on the OTG port. Mouse is working completely fine on standard USB port but due to some project specific reasons we need to use it over OTG.
Is there any other configuration which I need to do to get it working.
Thanks in Anticipation.
Regards,
Vishal.