Hi Support,
Currently, we use remoteproc to load the R5F firmware during Linux boot. That's, we copied the firmware file to the /lib/firmware/ Linux folder, and it's loaded during Linux boot.
The R5F runs bare-metal application. Our BSP is based on TI SDK 07.01.
I wonder if there is a way to load the R5F MCU firmware earlier, for example, in u-boot or even earlier?
We want the R5F MCU to start execution as early as possible after power up
Thanks