Follow the guide to set up ccs on ubuntu 22.04
Scripting console:
js:> loadJSfile ("/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js") Connecting to DMSC_Cortex_M3_0! Fill R5F ATCM memory... Writing While(1) for R5F Loading DMSC Firmware ... /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/soc/sysfw/binaries/ti-fs-firmware-j721e-gp.bin DMSC Firmware Load Done... DMSC Firmware run starting now... Running the DDR configuration... Wait till it completes! Connecting to MCU Cortex_R5_0! WKUP Boot Mode is 56 Main Boot Mode is 65 Disable MCU Timer for ROM clean up Error evaluating "GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f")": Unable to open file: /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f at GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f") (/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js#153) js:>
Console output stop at below, I think the problem is the path: /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/, sometimes the it start from system root: /home/user/, sometimes start from user's root.
DMSC_Cortex_M3_0: GEL Output: Setting DDR PLL + HSDIV to 933MHz DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80170000 DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80000E17 DMSC_Cortex_M3_0: GEL Output: DDR PLL + HSDIV set to 933MHz. DMSC_Cortex_M3_0: GEL Output: Frequency change request type 2 received from controller DMSC_Cortex_M3_0: GEL Output: Setting DDR PLL + HSDIV to 933MHz DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80170000 DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80000E18 DMSC_Cortex_M3_0: GEL Output: DDR PLL + HSDIV set to 933MHz. DMSC_Cortex_M3_0: GEL Output: --->>> All frequency change requests have completed... <<<--- DMSC_Cortex_M3_0: GEL Output: --->>> LPDDR4 Initialization is DONE! <<<--- MCU_Cortex_R5_0: GEL: Unable to open file: /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f
I changed the line replace with absolute path, then it can execute to next similar line of loading firmware.
if ((bootMode != 0x38) || (mainBootMode != 0x11)) { print("Disable MCU Timer for ROM clean up"); dsMCU1_0.memory.writeWord(0, 0x40400010, 0x1); /* Write reset to MCU Timer 0. Left running by ROM */ dsMCU1_0.memory.writeWord(0, 0x40F80430, 0xFFFFFFFF); /* Clear Pending Interrupts */ dsMCU1_0.memory.writeWord(0, 0x40F80018, 0x0); /* Clear Pending Interrupts */ // Reset the R5F to be in clean state. dsMCU1_0.target.reset(); // Load the board configuration init file. //dsMCU1_0.expression.evaluate('GEL_Load("'+ ccs_init_elf_file +'")'); dsMCU1_0.expression.evaluate('GEL_Load("/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f")'); // Run Asynchronously dsMCU1_0.target.runAsynch(); print ("Running Async"); // Halt the R5F and re-run. dsMCU1_0.target.halt(); }
js:> loadJSfile ("/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js") Connecting to DMSC_Cortex_M3_0! Fill R5F ATCM memory... Writing While(1) for R5F Loading DMSC Firmware ... /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/soc/sysfw/binaries/ti-fs-firmware-j721e-gp.bin DMSC Firmware Load Done... DMSC Firmware run starting now... Running the DDR configuration... Wait till it completes! Connecting to MCU Cortex_R5_0! WKUP Boot Mode is 56 Main Boot Mode is 65 Disable MCU Timer for ROM clean up Running Async Running the board configuration initialization from R5! Running DDR Memory Checks.... Clearing CLEC Secure Claim... ###################################################################################### Loading Sciserver Application on MCU1_0. This will service RM/PM messages If you do not want this to be loaded update the launch script to make loadSciserverFlag = 0 If you want to load and run other cores, please run the MCU1_0 core after Sciserver is loaded. ###################################################################################### Error evaluating "GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_freertos_mcu1_0_release.xer5f")": Unable to open file: /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_freertos_mcu1_0_release.xer5f at GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_freertos_mcu1_0_release.xer5f") (/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js#222) js:>
My question: Only I have this issue? is it OK on your side?