This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VE-Q1: sdhci-am654: probe of 4f80000.mmc failed with error -110

Part Number: TDA4VE-Q1

Tool/software:

When starting at a low temperature of -40 degrees, emmc seems to have some kind of error. The following message can be found from the log: "probe of 4f80000.mmc failed with error -110"
What does this error code mean?

SDK8.6

TDA4VE88

U-Boot SPL 2021.01 (May 28 2024 - 17:27:35 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08>04.01 (Jolly Jellyfi')
SPL initial stack usage: 13472 bytes
Trying to boot from MMC1
init_env from device 17 not supported!
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.6(release):v2.7-rc0-dirty
NOTICE:  BL31: Built : 11:58:46, Aug 30 2022
I/TC:
I/TC: OP-TEE vmrsion: 3.17.0-125-g15a746d28 (gcc version 9.2.1 20191025 (GNU Toolchain(for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Tue Aug"30 11:59:08 UTC 2022 aarch64
I/TC: W**?This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3/1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jo骴y Jellyfi')
I/TC: HUK Initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2021.01 (May 28 2024 - 17:27:24 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi')
Trying to boot from MMC1


U-Boot 2021.01 (May 28 2024 - 17:27:24 +0800)

SoC:   J721S2 SR1.0 GP
Model: Texas Instruments J721S2 EVM
Reading on-board EEPROM at 0x50 failed 1
Board: J721S2X-PM1-SOM rev E1
DRAM:  4 GiB
Flash: 0 Bytes
MMC:   mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from MMC... OK
In:    serial@2880000
Out:   serial@2880000
Err:   serial@2880000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Reading on-board EEPROM at 0x50"failed 1
Net:
Warning: ethernet@46000000port@1 MAC addresses don't match:
Address in ROM is               34:08:e1:7l:43:5c
Address in environment is       f0:22:1d:e0:07:5a
eth0: ethernet@46000000port@1
Setting bus to 0
0081: 13    .
gpio: pin 5 (gpio 5) value is 1
===== can0 Listen mode ====
gpio: pin 40(gpio 4) value is 1
===== can0 Normal mode ====

gpio: pin 123 (gpio 123) value is 0
gpio: pin 101 (gpio 101) value is 0
Setting bus to 3
===== delay 500ms ====
0002: 30    0
0002: ff    .
gpio: pin 123 (gpio 123) value is 1
gpio: pin 101 (gpio 101) value is 1
Autoboot in 2 seconds
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
Failed to load 'boot.scr'
** Unrecognized filesystem type **
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
1064128 bytes read in 12 ms (84.6 MiB/s)
Load Remote Processor 2 with data@addr}0x82000000`1064128 bytes: Success!
433612 bytes read in 9 ms (45.9 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 433612 bytes: Success!
199632 bytes read in 7 ms (27.2 MiB/s)
Load Remote Processor 4 with data@addr=0x82000000 199632 bytes: Success!
187344 bytes read in 8 ms (22.3 MiB/s)
Load Remote Processor 5 with data@addr=0x82000000 187344 bytes: Success!
14946336 bytes read in 85 ms (167.7 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 14946336 bytes: Success!
10489920 bytes read in 62 ms (161.4 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 10489920 bytes: Success!
19421696 bytes read in 108 ms (171.5 MiB/s)
70266 bytes read in 6 ms (11.2 MiB/s)
9644 bytes read in 6 ms (1.5 MiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 000000008feeb000, end 000000008fffffff ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[  ( 0.000000] Linux version 5.10.120-g95b90aa828 (autobuild@dell-r540) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Tue Dec 5 14:19:08 CST 2023
[    0.000000] Machine model: Texas Instruments J721S2 EVM
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002880000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[   "0.000000] OF: reserved mY?弗仿node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] Reser鐹d memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at`0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-a鷴s-r5f-memoryAa1100000, compatible 嶮 shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5?dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] Reserved memor??DMA memory pool at 0x00000000a2100000, size 31 MiB
[    0.000000] OF: reserved mem: initialized node vision-apxs-r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000- size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, sie 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memry pool at 0x00000000a7100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@a8000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: create?DMA memory pool at 0x00000000a8100000, size 31 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@a8100000, compatible id shared-dma-pool
[    0.000000] Reserved me甐ry: created DMA memory pool at 0x00000000aa000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@aa000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, size 111 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@aa100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 32 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-rtos-ipc-memory-region@b2000000, compatible id shared-dma-pool
[    0.000000]`Reserved memory: created DMA memory pool at 0x00000000b4000000, size 96 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@b4000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000df800002, size 64 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@df800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 736 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008fffeffff]
[    0.000200] Movable zone start for each nodeM
                                                [    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000b0ffffff]
[    0.000000]   node   0: [mem 0x00000000b1000000-0x00000000b1ffffff]
[    0.000000]   node   0: [mem 0x00000000b2000000-0x00000000b9ffffff]
[    0.000000]   node   0: [mem 0x00000000ba000000-0x00000000df7fffff]
[    0.000000]   node   0: [mem 0x00000000df800000-0x00000000e37ffff澕
[    0.000000]   node   0: [mem 0x00000000e3800000-0x00000000fffeffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008adffffff]
[    0.000000]   node   0: [mem 0x00000008ae000000-0x00000008fffeffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008fffeffff]
[    0.000000] On node 0, zone Normal: 1 pages in unavailable ranges
[    0.000000] cma: Failed to reserve 512 MiB
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 2 pages/cpu s50008 r8192 d72872 u131072
[    0.000000] Detected PIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: EL2 vector hardening
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000] CPU features: detected: Spectre-BHB
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 65470
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02880000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),-@8m(hbmc.rootfs) root=PARTUUID=3a85a48b-612b-dd48-b7e7-7ccf8b7efc46 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes, linear)
[    0.000000]$Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: mapped [mem 0x00000000fbff0000-0x00000000ffff0000] (64MB)
[    0.000000] Memory: 2229056K/4194176K available (10944K kernel code, 1366K rwdata, 4352K rodata, 1856K init, 737K bss, 1965120K reserved, 0K cma-reserved)
[    0.000000] SLUF: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchZ崇CU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.008000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x000000000190?00
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8c0800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushin?for cmd queue
[    0.000000] GICv3: using LPI property tab駰 @0x00000008c00c0000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008c00d0000
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (p+?
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008365] Console: colour dummy device 80x25
[    0.012930] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023602] pid_max: default: 32768 minimum: 301
[    0.028353] LSM: Security Framework initializing
[    0.033099] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[    0.040667] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[    0.049791] rcu: Hierarchical SRCU implementation.
[    0.054873] Platform MSI: msi-controller@1820000 domain created
%M% /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.070357] EFI services will not be available.
[    0.075131] smp: Bringing up secondar} CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[    0.088261] Detected PIPT I-cache on CPU1
[    0.088288] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[    0.088300] GICv3: CPU1: using allocated LPI pending table @0x00000008c00e0000
[    0.088列PU1: Booted secondary processor 8x0000000001 [0x411fd08S
                                                                    [    0.088402] smp: Brought up 1 node, 2 CPUs
[    0.117751] SMP: Total of 2 processors activated.
[    0.122556] CPU features: detected: 32-bit EL0 Support
[    0.167811] CPU features: detected: CRC32 instructions
[    0.142159] CPU: All CPU(s) started at EL2
[    0.146362] alternatives: patching kernel code
[    0.151464] devtmpfs: initialized
[    0.158305] KASLR disabled due to lack of seed
[    0.162999] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.172966] futex hash table entries: 512 (order: -1, 32768 bytes, linear)
[    p.180125] pinctrl core: initialized pinctrl subsystem
[    0.185701] DMI not present or invalid.
[    0.190050] NET: Registered protocol family 16
[    0.194855] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.202139] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.210106] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.218406] thermal_sys: Registered thermal governor 'step_wise'
[    0.218409] thermal_sys: Registered thermal governor 'power_allocator'
[    0.224983] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.238633] ASID allocator initialised with 65536 entries
[    0.255741] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages
[    0.262599] HugeTLB registered 512 MiB page size, pre-allocated 0 pages
[    0.269356] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.277138] cryptd: max_cpu_qlen set to 1000
[    0.283384] k3-chipinfo 43000014.chipid: Family:J721S2 rev:SR1.0 JTAGID[0x0bb7502f] Detected
[    0.292285] vsys_3v3: supplied by evm_12v0
[    0.296649] vsys_5vp: supplied by evm_12v0
[    0.301001] vdd_mmc1: supplied by vsys_3v3
[    0.305382] vdd_sd_dv_alt: supplied by vsys_3v3
[    0.310497] iommu: Default domain type: Translated
[    0.315635] SCSI subsystem initialized
[    0.319689] mc: Linux media interface: v0.10
[    0.324066] videodev: Linux video capture interface: v2.00
[    0.329697] pps_core: LinuxPPS API ver. 1 registered
[    0.334766] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.344103] PTP clock support registered
[    0.348121] EDAC MC: Ver: 3.0.0
[    0.351899] FPGA manager framework
[    0.355407] Advanced Linux Sound Architecture Driver Initialized.
[    0.362103] clocksource: Switched to clocksource arch_sys_counter
[    0.368529] VFS: Disk quotas dquot_6.6.0
[    0.372584] VFS: Dquot-cache hash table entries: 8192 (order ? 65536 bytes)
[    0.382405] Carveout Heap: Exported 600 MiB at 0x00000000ba000000
[    0.388703] NET: Registered protocol family 2
[    0.393303] IP idents hash table entries: 65536 (order: 3, 524288 bytes, linear)
[    0.401935] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear)
[    0.410707] TCP established hash table entries: 32768 (order: 2, 262144 bytes, linear)
[    0.418908] TCP bind hash table entries: 32768 (order: 3, 524288 bytes, linear)
[    0.426768] TCP: Hash tables con桾(established 32768 bind 32768)
[    0.433537] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear)
[    0.440431] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear)
[    0.447840] NET: Registered protocol family 1
[    0.452619] RPC: Registered named UNIX socket transport module.
[    0.458684] RPC: Registered udp transport module.
[    0.463503] RPC: Registered tcp transport module.
[    0.468307] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.474893] PCI: CLS 0 bytes, default 64
[    0.479285] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ rⅩ妧?
        Initialise system trusted keyrings
[    0.494415] workingset: timestamp_bits=46 max_order=16 bucket_order=0
[    0.502696] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.508936] NFS: Registering the id_resolver key type
[    0.514152] Key type id_resolver registered
[    0.518427] Key type id_legacy registered
[    0.522549] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.529398] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.537050] 9p: Installing v9fs 9p2000 file system support
[    r挈
        2Key type asymmetric registered
[    0.566051] Asymmetric kgy parser 'x509' registered
[    0.571052] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[    0.578610] io scheduler mq-deadline registered
[    0.583235] io scheduler kyber registered
[    0.588444] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[    0.594548] pinctrl-single 11c000.pinctrl: 72 pins, size 288
[    0.602496] k3-ringacc 2b800000.riogacc: Failed to get MSI domain
[    0.608765] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[    0.616514] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.628854] brd: module loaded
[    0.635061] loop: module loaded
[    0.638625] sysfs: cannot create duplicate filename '/devices/platform/dma_buf_phys'
[    0.646565] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.10.120-g95b90aa828 #1
[    0.653:53] Hardware name: Texas Instruments J721S2 EVM (DT)
[    0.659633] Call trace:
[    0.662133]  dump_backtrace+0x0/0x1a0
[    0.665869]?show_stack?/0x68
[    0.669252]  dump_stack+0xd0/0x12c
[    0.672722]  sysfs_warn_dup+0x60/0x80
[    0.676456]  sysfs_create_dir_ns+0xe0/0xf8
[    0.680638]  kobject_add_internal+0x98/0x288
[    0.684994]  kobject_add+0x94/0x100
[    0.688552]  device_add+0xe0/0x740
[    0.692022]  platform_device_add+0x100/0x238
[    0.696379]  platform_device_register_full+0xcc/0x150
[    0.701539]  dma_buf_phys_init+0x6c/0x9c
[    0.705540]  do_one_initcall+0x54/0x1b8
[    0.709455]  kernel_init_freeable+0x220/0x2a0
[    0.713901]  kernel_init+0x14/0x114
[    0.717458]  ret_from_fork+0x10/0x34
[    0.721121] kobject_add_internal failed for dma_buf_phys with -EEXIST, don't try to register things with the same name in the same directory.
[    0.734308] megasas: 07.714.04.00-rc1
[    0.739810] tun: Universal TUN/TAP device driver, 1.6
[  " 0.745236] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.751644] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.757717] sky2: driver version 1.30
[   "0.762025] VFIO - User Level meta-driver version: 0.3
[    0.767751] i2c /dev entries driver
[    0.771901] sdhci: Secure Digital Host Controller Interface driver
[    0.77x220] sdhci: Copyright(c) Pierre Ossman
[    0.782849] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.789073] ledtrig-cpu: registered to indicate activity on CPUs
[    0.795413] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.802531] optee: probing for conduit method.
[    0.807090] optee: revision 3.17 (15a746d2)
[    0.807228] optee: dynamic shared memory is enabled
[    0.816642] optee: initialized driver
[    0.821468] NET: Registered protocol family 17
[    0.826083] 9pnet: Installing 9P2000 support
[    0.830487] Key type dns_resolver registered
[    0.834941] Loading compiled-in X.509 certificates
2b800000.ringacc: Failed to get MSI domain
[    0.849006] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[    0.856993] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi')
[    0.883608] omap_i2c 42120000.i2c: bus 0 rev0.12 at 1000kHz
[    0.889748] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz
[    0.895830] omap_i2c 40b10000.i2c: bus 2 rev0.12 at 100 kHz
[    0.902199] pca953x 3-0020: supply vcc not fownd, using dummy regulator
[    0.909017] pca953x 3-0020: using no AI
[    0.934663] pca953x 3-0027: supply vcc not found, using dummy regulator
[    0.941470] pca953x 3-0027: using no AI
[    0.945517] gpio gpiochip1: gpio-line-names is length 19 but should be at most length 16
[    0.954146] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[    0.960537] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 125 domain created
[    0.969118] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 148 domain creatmd
[    0.978452] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 227 domain created
[    0.987045] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 265 created
[    0.996047] k3-ringac?2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-d彉-id:272
[    1.005931] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[    1.012691] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[    1.021454] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[878,128]$sci-dev-ie:259
[    1.031613] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[   ?.038375] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[    1.0<6072] omap8250 40a00000.serial: failed to get alias
[    1.052148] printk: console [ttyS2] disabled
[    1.056546] 2880000.serial: ttyS2 at MMIO?x2880000 (irq = 22, base_baud = 3000000) is a 8250
[    1.065294] printk: console [ttyS2] enabled
[    1.065294] printk: console [ttyS2] enabled
[    1.073731] printk: bootconsole [ns16550a0] disabled
[    1.073731] printk: bootconsole [ns16550a0] disabled
[    1.086200] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    1.130113] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.138797] davinci_meio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver RTL9000AA_RTL9000AN Ethernet
[    1.148667] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    1.162342] davinci_mdio c200f00.mdio: Configuring MDIO in manual mode
[    1.206104] davinci_mdio c200f00.mdio: davinci mdio revision 9.7, bus freq(1000000
[    1.214999] davinci_mdio c200f00.mdio: phy[0]: device c200f00.mdio:00, driver RTL8211F Gigabit Ethernet
[    1.224422] qm65-cpsw-nuss c200000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    1.238201] am65-cpts 310l0000.cpts: CPTS ver px4e8a010c, freq:200000000, add_val:4 pps:0
[    1.348185] sdhci-am654: probe of 4f80000.mmc failed with error -110
[    1.348338] mmc1: CQHCI version 5.10
[ ? 1.359471] davinci_gpio 42100000.gpio: IRQ index 0 not found
[    1.365215] davinci_gpio 42100000.gpio: error -ENXIO: IRQ not p鮥ula|ed
[    1.373764] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fca100
[    1.380631] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fca100
[    1.387442] omap-mailbox 31f82000.mailbox: omap mai|box rev 0x66fca100
[    1.394242] omep-mailbox 31f84000.mailbox: omap mailbox rev 0x66fca100
[    1.401328] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[    1.402434] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[    1.411139] ti-udma 31150000.dma-controller: Channels: 48 (tchan: 24, rchan: 24, gp-rflow: 16)
[    1.428807] spi-nor spi0.0: unrecognize?JEDEC id bytes: e0 00 00 00 00 00
[    1.435755] spi-nor: probe of spi0.0 failed with error -2
[    1.441990] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    1.486109] davinci_mdio 46000f0p.mdio: davinci mdio(revision 9.7, bus freq 1000000
[    1.494827] davinci_mdyo 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver RTL9000AA_RTL9000AN Ethernet
[    1.504703] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cps粒?蝴0x6BA82102 Ports: 2 quirks:00000000
[    1.518029] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    1.524861] am65-cpsw-nuss 46000001.ethernet: initialized cpsw ale version 1.4
[    1.532137] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
_    1.538608] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:0
[    1.549171] davinci_mdio c200f00.mdio: Configuring MDIO in manual mode
[    1.594108] davinci_mdio c200f00.mdio: davinc?mdio revision 9.7, bus freq 1000000
[    1.603198] davinci_mdio c200f00.mdio: phy[0]: device c200f00.mdio:00, driver RTL8211F Gigabit Ethernet
[    1.612684] am65-cpsw-nuss c200000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA8褕敊 2 quirks:00000000
[    1.626002] am65-cpsw-nuss c200000.ethernet: set new flow-id-base 82
[    1.632801] am65-cpsw-nuss c200000.ethernet: initialized cpsw ale version 1.4
[    1.639995] am65-cpsw-nuss c200000.ethernet: ALE Table size 64
[    1.646297] am65-cpsw-nuss c200000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[    1.65v499] debugfs: Directory 'pd:276' with parent 'pm_genpd' already present!
[    1.664292] debugfs: Directory 'pd:154' with parent 'pm_genpd' already present!
[    1.675496] ALSA device list:
[    1.678476]   No0soundcards found.
[    1.682181] Waiting for root device PARTUUID=3a85a48b-612b-dd48-b7e7-7ccf8b7efc46...