Other Parts Discussed in Thread: TMS320C6748
Tool/software:
Hello,
This is a follow up from original E2E link TMDSEMU560V2STM-U: TMDSEMU560V2STM-U - Processors forum - Processors - TI E2E support forums
No answer obtained from inquiry posted at TI E2E design support forums for the original delivery (attached).
Part# TMDSEMU560V2STM-U
Mouser PO# 029-7R890
Date code 2214
Can you please refer to detail provided below.
And check if possible to clarify if any concern to use TMDSEMU560V2STM-U with the target device TMS320C6748 ??
Or if any setup sequence required to be able to interface without problem ?
Please verify.
TMDSEMU560V2STM-U
TMS320C6748
Per customer:
the computer could not recognize the instrument when it was
connected, but this problem was resolved with the replacement.
The next time I tried to connect the instrument to the target device, the target
could not be recognized. The other instrument that I purchased with the
last one recognizes the target and works without any problems. The
computer used for evaluation and the target are the same.
Date: 05/16/24 Time: 12:36am »»
This replacement part was ok to connect PC but when customer changed to
connect to the target device cannot recognized.
One of the first order parts was no issue when customer connected to
target device. the computer used for evaluation and the target are the
same.