Tool/software:
Hi,
I've added WKUP UART0 to the device tree in Linux, and set the baud rate to 9600 in Linux using stty -F /ttySn. When I use the third COM port to interact with the serial port, I need to set it at twice the baud rate (19200) to transmit and receive data correctly. What could be the cause of this issue?