This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: Unable to Access SPI Interface from 40-Pin Expansion Connector on AM62xx EVM Running Debian OS

Part Number: SK-AM62
Other Parts Discussed in Thread: AM625,

Tool/software:

Hello TI team,

I am working with the AM625 Evaluation Module (EVM) and running Debian OS on the processor. My goal is to access the SPI interface from the 40-pin expansion connector and also i want to enable two SPI lines. However, I am unable to see any SPI-related devices under /dev/ that would indicate the presence of SPI interfaces.

I am new to using this device and Linux OS, so any guidance or pointers to relevant documentation would be greatly appreciated. Can someone provide a step-by-step guide on how to enable and access the SPI interface from the 40-pin expansion connector in Debian OS?

Thank You

Kasun

  • Hi Kasun,

    we don't have a specific "step by step guide" for Debian but this is really a Kernel and Kernel-configuration (Device Tree)-related concern so anything we have on "Linux SPI" really applies here. Debian-specific differences would be how to deploy/integrate updated Kernel / Device Tree Files but that hopefully shouldn't be too difficult to figure out (our Debian SDK documentation would be a good starting point).

    Assuming you want to do what's called "Usermode SPI", s for using Linux / SPI see...

    1. See the "Linux Userspace Interface" section in the AM62x Linux SDK documentation for a general starting point, and how to enable a required Kernel configuration:
      https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_02_01_10/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/SPI.html
    2. For how to make the needed Device Tree changes (and common issues related to this), see this E2E post/thread here:
      https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1263441/sk-am62-no-spi-signals-on-expansion-headers/4783737

    Regards, Andreas

  • Hi Andreas,

    Thank you for your response.

    I'll try and make an update on this.

    Regards,
    Kasun

  • Hi Andreas, 

    I am currently working with an AM62xx Evaluation Module (EVM) and using the 09.02.01.10 SDK (dated 22 May 2024) along with the tisdk-debian-bookworm-am62xx-evm.wic.xz operating system. 

    In the kernel configuration file, CONFIG_SPI_SPIDEV=m is set as default. Additionally, config.gz does not allow modifications. The following are the relevant Device Tree Blob Overlay (DTBO) files located in the /boot/dtb/ti directory. The device tree file for my processor board is k3-am625-sk.dtb. 

    root@am62xx-evm:/boot/dtb/ti# ls  

    k3-am62-lp-sk-lincolntech-lcd185-panel.dtbo
    k3-am62-lp-sk-microtips-mf101hie-panel.dtbo
    k3-am62-lp-sk-nand.dtbo
    k3-am62-lp-sk.dtb
    k3-am625-beagleplay-csi2-ov5640.dtbo
    k3-am625-beagleplay-csi2-tevi-ov5640.dtbo
    k3-am625-beagleplay-lincolntech-lcd185-panel.dtbo
    k3-am625-beagleplay.dtb
    k3-am625-sk-dmtimer-pwm.dtbo
    k3-am625-sk-ecap-capture.dtbo
    k3-am625-sk-lincolntech-lcd185-panel.dtbo
    k3-am625-sk-mcspi-loopback.dtbo
    k3-am625-sk-microtips-mf101hie-panel.dtbo
    k3-am625-sk-microtips-mf103hie-lcd2.dtbo
    k3-am625-sk-pwm.dtbo
    k3-am625-sk-rpi-hdr-ehrpwm.dtbo
    k3-am625-sk.dtb
    k3-am62a7-sk-csi2-imx219.dtb
    k3-am62a7-sk-csi2-ox05b1s.dtbo
    k3-am62a7-sk-e3-max-opp.dtbo
    k3-am62a7-sk-ethernet-dc01.dtbo
    k3-am62a7-sk-fusion-imx390.dtb
    k3-am62a7-sk-fusion-ov2312.dtb
    k3-am62a7-sk-rpi-hdr-ehrpwm.dtbo
    k3-am62a7-sk-ub954-evm-ov2312.dtb
    k3-am62p5-sk-dsi-rpi-7inch-panel.dtbo
    k3-am62p5-sk-dss-shared-mode.dtbo
    k3-am62p5-sk-eqep.dtbo
    k3-am62p5-sk-mcan.dtbo
    k3-am62p5-sk-microtips-mf101hie-panel.dtbo
    k3-am62p5-sk-microtips-mf103hie-lcd2.dtbo
    k3-am62p5-sk-rpi-hdr-ehrpwm.dtbo
    k3-am62p5-sk.dtb
    k3-am62x-sk-csi2-imx219.dtbo
    k3-am62x-sk-csi2-ov5640.dtbo
    k3-am62x-sk-csi2-tevi-ov5640.dtbo
    k3-am62x-sk-csi2-v3link-fusion.dtbo
    k3-am62x-sk-eqep.dtbo
    k3-am62x-sk-hdmi-audio.dtbo
    k3-am62x-sk-hdmi-disable-fastboot.dtbo
    k3-am62x-sk-lpm-wkup-sources.dtbo
    k3-am62x-sk-mcan.dtbo
    k3-am642-evm-icssg1-dualemac-mii.dtbo
    k3-am642-evm-icssg1-dualemac.dtbo
    k3-am642-evm-nand.dtbo
    k3-am642-evm.dtb
    k3-am642-sk.dtb
    k3-am6528-iot2050-basic-pg2.dtb
    k3-am6528-iot2050-basic.dtb
    k3-am654-base-board.dtb
    k3-am654-evm-oldi-lcd1evm.dtbo
    k3-am654-idk.dtbo
    k3-am654-pcie-usb2.dtbo
    k3-am654-pcie-usb3.dtbo
    k3-am6548-iot2050-advanced-pg2.dtb
    k3-am6548-iot2050-advanced.dtb
    k3-am68-sk-base-board.dtb
    k3-am68-sk-bb-csi2-ov5640.dtbo
    k3-am68-sk-bb-rpi-cam-imx219.dtbo
    k3-am68-sk-fpdlink-fusion.dtbo
    k3-am68-sk-rpi-hdr-ehrpwm.dtbo
    k3-am68-sk-som-ddr-mem-carveout.dtbo
    k3-am68-sk-v3link-fusion.dtbo
    k3-am69-sk-csi2-ov5640.dtbo
    k3-am69-sk-csi2-rpi-cam-imx219.dtbo
    k3-am69-sk-csi2-v3link-fusion.dtbo
    k3-am69-sk-ddr-mem-carveout.dtbo
    k3-am69-sk-fpdlink-fusion-auxport.dtbo
    k3-am69-sk-fpdlink-fusion.dtbo
    k3-am69-sk-rpi-hdr-ehrpwm.dtbo
    k3-am69-sk.dtb
    k3-fpdlink-imx390-rcm-0-0.dtbo
    k3-fpdlink-imx390-rcm-0-1.dtbo
    k3-fpdlink-imx390-rcm-0-2.dtbo
    k3-fpdlink-imx390-rcm-0-3.dtbo
    k3-fpdlink-imx390-rcm-1-0.dtbo
    k3-fpdlink-imx390-rcm-1-1.dtbo
    k3-fpdlink-imx390-rcm-1-2.dtbo
    k3-fpdlink-imx390-rcm-1-3.dtbo
    k3-fpdlink-imx390-rcm-2-0.dtbo
    k3-fpdlink-imx390-rcm-2-1.dtbo
    k3-fpdlink-imx390-rcm-2-2.dtbo
    k3-fpdlink-imx390-rcm-2-3.dtbo
    k3-fpdlink-ov2312-0-0.dtbo
    k3-fpdlink-ov2312-0-1.dtbo
    k3-fpdlink-ov2312-0-2.dtbo
    k3-fpdlink-ov2312-0-3.dtbo
    k3-j7200-evm-mcspi-loopback.dtbo
    k3-j7200-evm-virt-mac-client.dtbo
    k3-j7200-evm.dtb
    k3-j721e-beagleboneai64-dsi-rpi-7inch-panel.dtbo
    k3-j721e-beagleboneai64.dtb
    k3-j721e-common-proc-board-infotainment.dtbo
    k3-j721e-evm-csi2-ov5640.dtbo
    k3-j721e-evm-fusion.dtbo
    k3-j721e-evm-gesi-exp-board.dtbo
    k3-j721e-evm-pcie0-ep.dtbo
    k3-j721e-evm-virt-mac-client.dtbo
    k3-j721e-evm.dtb
    k3-j721e-sk-csi2-ov5640.dtbo
    k3-j721e-sk-csi2-rpi-imx219.dtbo
    k3-j721e-sk-fusion.dtbo
    k3-j721e-sk-rpi-hdr-ehrpwm.dtbo
    k3-j721e-sk.dtb
    k3-j721s2-common-proc-board.dtb
    k3-j721s2-evm-csi2-ov5640.dtbo
    k3-j721s2-evm-fusion.dtbo
    k3-j721s2-evm-gesi-exp-board.dtbo
    k3-j721s2-evm-pcie1-ep.dtbo
    k3-j722s-evm-csi2-ov5640.dtbo
    k3-j722s-evm-csi2-rpi-cam-imx219.dtbo
    k3-j722s-evm-csi2-tevi-ov5640.dtbo
    k3-j722s-evm-dsi-rpi-7inch-panel.dtbo
    k3-j722s-evm-fpdlink-fusion.dtbo
    k3-j722s-evm-microtips-mf101hie-panel.dtbo
    k3-j722s-evm-v3link-fusion.dtbo
    k3-j722s-evm.dtb
    k3-j784s4-evm-csi2-ov5640.dtbo
    k3-j784s4-evm-quad-port-eth-exp1.dtbo
    k3-j784s4-evm-usxgmii-exp1-exp2.dtbo
    k3-j784s4-evm-virt-mac-client.dtbo
    k3-j784s4-evm.dtb
    k3-v3link-imx219-0-0.dtbo
    k3-v3link-imx219-0-1.dtbo
    k3-v3link-imx219-0-2.dtbo
    k3-v3link-imx219-0-3.dtbo

     I have decompiled the k3-am625-sk.dtb using the device-tree-compiler installed via apt (the decompiled file is attached). 

    On the E2E forum(https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1263441/sk-am62-no-spi-signals-on-expansion-headers/4783737), it was suggested to add the following configuration to the Device Tree Blob (DTB) and compile it: 

    .............................................................................................................................. 

    main_spi0_pins_default: main-spi0-pins-default {  
       pinctrl-single,pins = <  
           AM62X_IOPAD(0x01bc, PIN_OUTPUT, 0) /* (A14) SPI0_CLK */  
           AM62X_IOPAD(0x01c0, PIN_OUTPUT, 0) /* (B13) SPI0_D0 */  
           AM62X_IOPAD(0x01c4, PIN_INPUT, 0) /* (B14) SPI0_D1 */  
           AM62X_IOPAD(0x01b4, PIN_OUTPUT, 0) /* (A13) SPI0_CS0 */  
       >;  
    };  
     
    &spi1 {  
       status = "okay";  
       pinctrl-names = "default";  
       pinctrl-0 = <&spi1_pins_s0>;  
       spidev@1 {  
           spi-max-frequency = <24000000>;  
           reg = <0>;  
           compatible = "rohm,dh2228fv";  
       };  
    }; 
     

    ..................................................................................................................

    However, I am unsure where exactly to place above configuration within the DTB. Additionally, I would appreciate some clarification on the purpose of the k3-am625-sk-mcspi-loopback.dtbo file. 

    Could you please provide guidance on resolving this issue? I am new to working with this processor board and Linux kernel configurations.Please provide step-by-step guidance.

    Thank you for your assistance. 

    Best regards, 

    Kasun 

    7357.DTS.txt

  • In the kernel configuration file, CONFIG_SPI_SPIDEV=m is set as defau

    If it is set to be build as a module it should work, the driver ("module") will get loaded as the device tree is being parsed and processed.

    However, I am unsure where exactly to place above configuration within the DTB.

    You can just add this section to the k3-am625-sk.dts original source file directly, and then compile this source file. This is best done in the context of the Linux kernel source used for the Debian SDK. The Debian SDK User's Guide has steps that show how to re-build the kernel package so you can just follow this in order to build a kernel package that has the device tree you updated: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_02_01_Debian/exports/docs/debian/Building_Debian_Packages.html

    Additionally, I would appreciate some clarification on the purpose of the k3-am625-sk-mcspi-loopback.dtbo file. 

    You can use U-Boot to apply this overlay file on top of another device tree blob (such as k3-am625-sk.dtb), effectively merging the two in binary context. To do that stop U-Boot so you get the prompt, and enter...

    => env set name_overlays k3-am625-sk.dtb

    ...and then start the boot process using...

    => boot

    This should establish a basic working SPI configuration you can exercise using userspace applications (such as spidev_test.c, that comes with the kernel).

    Regards, Andreas

  • Hi Andreas,

    Thank you for the valuable response. It was very helpful.

    I successfully enabled the SPIDEV interface and tested the SPI0 channel using the spidev_test.c with a loopback configuration. The spidev1.0 device appears in the /dev/ directory. Below are the steps I followed:

    => env set name_overlays k3-am625-sk.dtb k3-am625-sk-mcspi-loopback.dtbo
    => boot

    Upon connecting spi0_D1 and spi0_D0 together, I obtained the following results:

    spi mode: 0x0
    bits per word: 8
    max speed: 500000 Hz (500 kHz)
    TX | FF FF FF FF FF FF FF FF FF FF
    RX | FF FF FF FF FF FF FF FF FF FF

    I guess,this confirms that the SPI0 channel is configured and working properly. Below is the content of the k3-am625-sk-mcspi-loopback.dts:

    ............................................................................................................................................................................

    /dts-v1/;

    / {

    fragment@0 {
    target = <0xffffffff>;

    __overlay__ {

    main-spi0-pins-default {
    pinctrl-single,pins = <0x1bc 0x50000 0x1c0 0x50000 0x1c4 0x50000 0x1b4 0x50000>;
    phandle = <0x01>;
    };
    };
    };

    fragment@1 {
    target = <0xffffffff>;

    __overlay__ {

    gpio@22 {

    en_rpi_3v3 {
    gpio-hog;
    gpios = <0x05 0x00>;
    output-high;
    line-name = "EXP_PS_3V3_EN";
    };
    };
    };
    };

    fragment@2 {
    target = <0xffffffff>;

    __overlay__ {
    status = "okay";
    #address-cells = <0x01>;
    #size-cells = <0x00>;
    pinctrl-0 = <0x01>;
    pinctrl-names = "default";

    spidev@0 {
    compatible = "rohm,dh2228fv";
    spi-max-frequency = <0x16e3600>;
    reg = <0x00>;
    };
    };
    };

    __fixups__ {
    main_pmx0 = "/fragment@0:target:0";
    main_i2c1 = "/fragment@1:target:0";
    main_spi0 = "/fragment@2:target:0";
    };

    __local_fixups__ {

    fragment@2 {

    __overlay__ {
    pinctrl-0 = <0x00>;
    };
    };
    };
    }
    .............................................................................................................................................

    Now, I would like to enable the SPI2 channel in the EXPANSION HEADER of 40 pin. I need to enable both spi0 and spi2. Is there a straightforward and proper method to do this? I am also unsure how the hex values (e.g., pinctrl-single,pins = <0x1bc 0x50000 0x1c0 0x50000 0x1c4 0x50000 0x1b4 0x50000>;) were derived in the above shown k3-am625-sk-mcspi-loopback.dts.

    Can I modify the above k3-am625-sk-mcspi-loopback.dts to enable SPI2 with its pin configurations? If so, what specific changes should be made to the k3-am625-sk-mcspi-loopback.dts?

    Any guidance on this matter would be greatly appreciated.

    Thank you.

    Best regards,

    Kasun

  • Now, I would like to enable the SPI2 channel in the EXPANSION HEADER of 40 pin. I need to enable both spi0 and spi2. Is there a straightforward and proper method to do this?

    You can follow what was done in this post here and edit the DTS source file accordingly: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1249053/am625-testing-spi-interface-on-am625-based-custom-board/4752269#4752269  It shows how to setup both the needed pinmux and additions needed to enable the main_spi2 node.

    Regards, Andreas

  • Hi Andreas,

    Thank you very much for the reply.  

    SPI0 was successfully enabled using k3-am625-sk-mcspi-loopback.dtbo. “saveenv” is also not working in U-Boot. So it is not permanent. after a normal reboot spidev1.0 is not in /dev/. 

     In this (https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1263441/sk-am62-no-spi-signals-on-expansion-headers/4783737) thread, It is mentioned that they have build the device tree using k3-am62x-sk-common.dtsi.But /boot/dtb/ti/k3-am62x-sk-common.dtb not exits in our Debian OS. 
     

    Is it required to build the kernel again by using SDK? But we tried to build the kernel using “make linux”, but errors came. Provide some guidance. Other thing is it enough to change the k3-am62x-sk-common.dtsi and build the kernel to enable spi? 

    ---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

    Our goal is to enable both spi0 and spi2 in expansion header of 40 pin. 

    We changed k3-am625-sk-mcspi-loopback.dtbo for spi2 same as spi0 as shown below. 

    /dts-v1/; 
     
    / { 
     
    fragment@0 { 
    target = <0xffffffff>; 
     
    __overlay__ { 
     
    main-spi0-pins-default { 
    pinctrl-single,pins = <0x1b0 0x50000 0x198 0x50000 0x194 0x50000 0x1ac 0x50000>; 
    phandle = <0x01>; 
    }; 
    }; 
    }; 
     
    fragment@1 { 
    target = <0xffffffff>; 
     
    __overlay__ { 
     
    gpio@22 { 
     
    en_rpi_3v3 { 
    gpio-hog; 
    gpios = <0x05 0x00>; 
    output-high; 
    line-name = "EXP_PS_3V3_EN"; 
    }; 
    }; 
    }; 
    }; 
     
    fragment@2 { 
    target = <0xffffffff>; 
     
    __overlay__ { 
    status = "okay"; 
    #address-cells = <0x01>; 
    #size-cells = <0x00>; 
    pinctrl-0 = <0x01>; 
    pinctrl-names = "default"; 
     
    spidev@2 { 
    compatible = "rohm,dh2228fv"; 
    spi-max-frequency = <0x16e3600>; 
    reg = <0x00>; 
    }; 
    }; 
    }; 
     
    __fixups__ { 
    main_pmx0 = "/fragment@0:target:0"; 
    main_i2c1 = "/fragment@1:target:0"; 
    main_spi2 = "/fragment@2:target:0"; 
    }; 
     
    __local_fixups__ { 
     
    fragment@2 { 
     
    __overlay__ { 
    pinctrl-0 = <0x00>; 
    }; 
    }; 
    }; 
    } 

    After compiling the overlay k3-am625-sk-mcspi-loopback.dtbo was added from the U-boot (same did for spi0) spidev1.0 was /dev/.  

    Why spidev1.2 is not created? 

    We observed from logic analyzer. But nothing happen for spi2_clk, spi2_CS0, spi2_cs2, spi2_d0, and spi2_d1. 

    As in link(https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1350774/sk-am62-main-domain-spi-channel-two/5176728#5176728 ), we tried from CCS, It was successful for below configurations. 

    FETBUF_EN =1 

    FET_SEL =0 

    Could you please provide the necessary guidance to achieve our goal of enabling spi0 and spi2 from tisdk-debian-bookworm-am62xx-evm.wic.xz operating system in same time. 

    Best Regards, 

    Kasun 

     

     

      

     

     

  • Can you share your .dts* source file please?

    Regards, Andreas

  • Hi Kasun,

    no I was asking for the actual source files, not the de-compiled source files. Usually this is a combination of things taken from the Kernel tree (from arch/arm64/boot/dts/ti/), plus your modifications

    Regards, Andreas

  • Hi Andreas,

    // SPDX-License-Identifier: GPL-2.0
    /*
     * AM625 SK: https://www.ti.com/lit/zip/sprr448
     *
     * Copyright (C) 2021-2022 Texas Instruments Incorporated - https://www.ti.com/
     */
    
    /dts-v1/;
    
    #include "k3-am62x-sk-common.dtsi"
    
    / {
    	compatible = "ti,am625-sk", "ti,am625";
    	model = "Texas Instruments AM625 SK";
    
    	opp-table {
    		/* Add 1.4GHz OPP for am625-sk board. Requires VDD_CORE to be at 0.85V */
    		opp-1400000000 {
    			opp-hz = /bits/ 64 <1400000000>;
    			opp-supported-hw = <0x01 0x0004>;
    			clock-latency-ns = <6000000>;
    		};
    	};
    
    	memory@80000000 {
    		device_type = "memory";
    		/* 2G RAM */
    		reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
    
    	};
    
    	vmain_pd: regulator-0 {
    		/* TPS65988 PD CONTROLLER OUTPUT */
    		compatible = "regulator-fixed";
    		regulator-name = "vmain_pd";
    		regulator-min-microvolt = <5000000>;
    		regulator-max-microvolt = <5000000>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vcc_5v0: regulator-1 {
    		/* Output of LM34936 */
    		compatible = "regulator-fixed";
    		regulator-name = "vcc_5v0";
    		regulator-min-microvolt = <5000000>;
    		regulator-max-microvolt = <5000000>;
    		vin-supply = <&vmain_pd>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vcc_3v3_sys: regulator-2 {
    		/* output of LM61460-Q1 */
    		compatible = "regulator-fixed";
    		regulator-name = "vcc_3v3_sys";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		vin-supply = <&vmain_pd>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vdd_mmc1: regulator-3 {
    		/* TPS22918DBVR */
    		compatible = "regulator-fixed";
    		regulator-name = "vdd_mmc1";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		regulator-boot-on;
    		enable-active-high;
    		vin-supply = <&vcc_3v3_sys>;
    		gpio = <&exp1 3 GPIO_ACTIVE_HIGH>;
    	};
    
    	vdd_sd_dv: regulator-4 {
    		/* Output of TLV71033 */
    		compatible = "regulator-gpio";
    		regulator-name = "tlv71033";
    		pinctrl-names = "default";
    		pinctrl-0 = <&vdd_sd_dv_pins_default>;
    		regulator-min-microvolt = <1800000>;
    		regulator-max-microvolt = <3300000>;
    		regulator-boot-on;
    		vin-supply = <&vcc_5v0>;
    		gpios = <&main_gpio0 31 GPIO_ACTIVE_HIGH>;
    		states = <1800000 0x0>,
    			 <3300000 0x1>;
    	};
    
    	vcc_1v8: regulator-5 {
    		/* output of TPS6282518DMQ */
    		compatible = "regulator-fixed";
    		regulator-name = "vcc_1v8";
    		regulator-min-microvolt = <1800000>;
    		regulator-max-microvolt = <1800000>;
    		vin-supply = <&vcc_3v3_sys>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	wlan_lten: regulator-6 {
    		compatible = "regulator-fixed";
    		regulator-name = "wlan_lten";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		vin-supply = <&vcc_3v3_sys>;
    		gpios = <&exp1 11 GPIO_ACTIVE_LOW>;
    	};
    
    	wlan_en: regulator-7 {
    		compatible = "regulator-fixed";
    		regulator-name = "wlan_en";
    		regulator-min-microvolt = <1800000>;
    		regulator-max-microvolt = <1800000>;
    		vin-supply = <&wlan_lten>;
    		enable-active-high;
    		gpios = <&main_gpio0 71 GPIO_ACTIVE_HIGH>;
    		pinctrl-names = "default";
    		pinctrl-0 = <&wlan_en_pins_default>;
    	};
    
    	vdd_core: regulator-8 {
    		/* output of TPS62826DMQ */
    		compatible = "regulator-fixed";
    		regulator-name = "vdd_core";
    		regulator-min-microvolt = <850000>;
    		regulator-max-microvolt = <850000>;
    		vin-supply = <&vcc_3v3_sys>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    };
    
    &main_pmx0 {
    	main_rgmii2_pins_default: main-rgmii2-pins-default {
    		pinctrl-single,pins = <
    			AM62X_IOPAD(0x184, PIN_INPUT, 0) /* (AE23) RGMII2_RD0 */
    			AM62X_IOPAD(0x188, PIN_INPUT, 0) /* (AB20) RGMII2_RD1 */
    			AM62X_IOPAD(0x18c, PIN_INPUT, 0) /* (AC21) RGMII2_RD2 */
    			AM62X_IOPAD(0x190, PIN_INPUT, 0) /* (AE22) RGMII2_RD3 */
    			AM62X_IOPAD(0x180, PIN_INPUT, 0) /* (AD23) RGMII2_RXC */
    			AM62X_IOPAD(0x17c, PIN_INPUT, 0) /* (AD22) RGMII2_RX_CTL */
    			AM62X_IOPAD(0x16c, PIN_OUTPUT, 0) /* (Y18) RGMII2_TD0 */
    			AM62X_IOPAD(0x170, PIN_OUTPUT, 0) /* (AA18) RGMII2_TD1 */
    			AM62X_IOPAD(0x174, PIN_OUTPUT, 0) /* (AD21) RGMII2_TD2 */
    			AM62X_IOPAD(0x178, PIN_OUTPUT, 0) /* (AC20) RGMII2_TD3 */
    			AM62X_IOPAD(0x168, PIN_OUTPUT, 0) /* (AE21) RGMII2_TXC */
    			AM62X_IOPAD(0x164, PIN_OUTPUT, 0) /* (AA19) RGMII2_TX_CTL */
    		>;
    	};
    
    	ospi0_pins_default: ospi0-pins-default {
    		pinctrl-single,pins = <
    			AM62X_IOPAD(0x000, PIN_OUTPUT, 0) /* (H24) OSPI0_CLK */
    			AM62X_IOPAD(0x02c, PIN_OUTPUT, 0) /* (F23) OSPI0_CSn0 */
    			AM62X_IOPAD(0x00c, PIN_INPUT, 0) /* (E25) OSPI0_D0 */
    			AM62X_IOPAD(0x010, PIN_INPUT, 0) /* (G24) OSPI0_D1 */
    			AM62X_IOPAD(0x014, PIN_INPUT, 0) /* (F25) OSPI0_D2 */
    			AM62X_IOPAD(0x018, PIN_INPUT, 0) /* (F24) OSPI0_D3 */
    			AM62X_IOPAD(0x01c, PIN_INPUT, 0) /* (J23) OSPI0_D4 */
    			AM62X_IOPAD(0x020, PIN_INPUT, 0) /* (J25) OSPI0_D5 */
    			AM62X_IOPAD(0x024, PIN_INPUT, 0) /* (H25) OSPI0_D6 */
    			AM62X_IOPAD(0x028, PIN_INPUT, 0) /* (J22) OSPI0_D7 */
    			AM62X_IOPAD(0x008, PIN_INPUT, 0) /* (J24) OSPI0_DQS */
    		>;
    	};
    
    	vdd_sd_dv_pins_default: vdd-sd-dv-pins-default {
    		pinctrl-single,pins = <
    			AM62X_IOPAD(0x07c, PIN_OUTPUT, 7) /* (P25) GPMC0_CLK.GPIO0_31 */
    		>;
    	};
    
    	main_gpio1_ioexp_intr_pins_default: main-gpio1-ioexp-intr-pins-default {
    		pinctrl-single,pins = <
    			AM62X_IOPAD(0x01d4, PIN_INPUT, 7) /* (B15) UART0_RTSn.GPIO1_23 */
    		>;
    	};
    
    	wlan_en_pins_default: wlan-en-pins-default {
    		pinctrl-single,pins = <
    				AM62X_IOPAD(0x124, PIN_OUTPUT, 7) /* (A23) MMC2_SDCD.GPIO0_71 */
    		>;
    	};
    
    	main_mmc2_pins_default: main-mmc2-pins-default {
    		pinctrl-single,pins = <
    			AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */
    			AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */
    			AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */
    			AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */
    			AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */
    			AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */
    			AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */
    		>;
    	};
    
    	main_wlirq_pins_default: main-wlirq-pins-default {
    		pinctrl-single,pins = <
    			AM62X_IOPAD(0x128, PIN_INPUT, 7) /* (B23) MMC2_SDWP.GPIO0_72 */
    		>;
    	};
    };
    
    &main_i2c1 {
    	exp1: gpio@22 {
    		compatible = "ti,tca6424";
    		reg = <0x22>;
    		gpio-controller;
    		#gpio-cells = <2>;
    		gpio-line-names = "GPIO_CPSW2_RST", "GPIO_CPSW1_RST",
    				   "PRU_DETECT", "MMC1_SD_EN",
    				   "VPP_LDO_EN", "EXP_PS_3V3_En",
    				   "EXP_PS_5V0_En", "EXP_HAT_DETECT",
    				   "GPIO_AUD_RSTn", "GPIO_eMMC_RSTn",
    				   "UART1_FET_BUF_EN", "WL_LT_EN",
    				   "GPIO_HDMI_RSTn", "CSI_GPIO1",
    				   "CSI_GPIO2", "PRU_3V3_EN",
    				   "HDMI_INTn", "PD_I2C_IRQ",
    				   "MCASP1_FET_EN", "MCASP1_BUF_BT_EN",
    				   "MCASP1_FET_SEL", "UART1_FET_SEL",
    				   "TSINT#", "IO_EXP_TEST_LED";
    
    		interrupt-parent = <&main_gpio1>;
    		interrupts = <23 IRQ_TYPE_EDGE_FALLING>;
    		interrupt-controller;
    		#interrupt-cells = <2>;
    
    		pinctrl-names = "default";
    		pinctrl-0 = <&main_gpio1_ioexp_intr_pins_default>;
    	};
    };
    
    &sdhci1 {
    	vmmc-supply = <&vdd_mmc1>;
    	vqmmc-supply = <&vdd_sd_dv>;
    };
    
    &sdhci2 {
    	status = "okay";
    	vmmc-supply = <&wlan_en>;
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_mmc2_pins_default>;
    	bus-width = <4>;
    	non-removable;
    	ti,fails-without-test-cd;
    	cap-power-off-card;
    	keep-power-in-suspend;
    	assigned-clocks = <&k3_clks 157 158>;
    	assigned-clock-parents = <&k3_clks 157 160>;
    
    	#address-cells = <1>;
    	#size-cells = <0>;
    	wlcore: wlcore@2 {
    		compatible = "ti,wl1837";
    		reg = <2>;
    		pinctrl-names = "default";
    		pinctrl-0 = <&main_wlirq_pins_default>;
    		interrupt-parent = <&main_gpio0>;
    		interrupts = <72 IRQ_TYPE_EDGE_RISING>;
    	};
    };
    
    &cpsw3g {
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_rgmii1_pins_default
    		     &main_rgmii2_pins_default>;
    
    	cpts@3d000 {
    		/* MAP HW3_TS_PUSH to GENF1 */
    		ti,pps = <2 1>;
    	};
    };
    
    &cpsw_port2 {
    	phy-mode = "rgmii-rxid";
    	phy-handle = <&cpsw3g_phy1>;
    };
    
    &cpsw3g_mdio {
    	cpsw3g_phy1: ethernet-phy@1 {
    		reg = <1>;
    		ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
    		ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
    		ti,min-output-impedance;
    	};
    };
    
    &ospi0 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&ospi0_pins_default>;
    
    	flash@0{
    		compatible = "jedec,spi-nor";
    		reg = <0x0>;
    		spi-tx-bus-width = <8>;
    		spi-rx-bus-width = <8>;
    		spi-max-frequency = <25000000>;
    		cdns,tshsl-ns = <60>;
    		cdns,tsd2d-ns = <60>;
    		cdns,tchsh-ns = <60>;
    		cdns,tslch-ns = <60>;
    		cdns,read-delay = <4>;
    
    		partitions {
    			compatible = "fixed-partitions";
    			#address-cells = <1>;
    			#size-cells = <1>;
    
    			partition@0 {
    				label = "ospi.tiboot3";
    				reg = <0x0 0x80000>;
    			};
    
    			partition@80000 {
    				label = "ospi.tispl";
    				reg = <0x80000 0x200000>;
    			};
    
    			partition@280000 {
    				label = "ospi.u-boot";
    				reg = <0x280000 0x400000>;
    			};
    
    			partition@680000 {
    				label = "ospi.env";
    				reg = <0x680000 0x40000>;
    			};
    
    			partition@6c0000 {
    				label = "ospi.env.backup";
    				reg = <0x6c0000 0x40000>;
    			};
    
    			partition@800000 {
    				label = "ospi.rootfs";
    				reg = <0x800000 0x37c0000>;
    			};
    
    			partition@3fc0000 {
    				label = "ospi.phypattern";
    				reg = <0x3fc0000 0x40000>;
    			};
    		};
    	};
    };
    
    &tlv320aic3106 {
    	DVDD-supply = <&vcc_1v8>;
    };
    
    #define K3_TS_OFFSET(pa, val)	(0x4+(pa)*4) (0x10000 | val)
    
    &timesync_router {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&cpsw_cpts>;
    
    	/* Use Time Sync Router to map GENF1 input to HW3_TS_PUSH output */
    	cpsw_cpts: cpsw-cpts {
    		pinctrl-single,pins = <
    			/* pps [cpsw cpts genf1] in17 -> out12 [cpsw cpts hw3_push] */
    			K3_TS_OFFSET(12, 17)
    			>;
    	};
    };

    Regards,

    Kasun

  • Hi Kasun,

    thanks but what you sent looks like the standard top-level device tree file for the SK-AM62B board as provided by TI. I don't see any SPI-related modifications in there which I guess makes sense since you are working with the overlay file. So can you please send the source of the overlay file that you modified? To clarify, what I'm expecting is a device tree overlay file (usually named *.dtso) with your modification added in, just like the example one that TI provides, see https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/arch/arm64/boot/dts/ti/k3-am625-sk-mcspi-loopback.dtso?h=ti-linux-6.1.y

    Regards, Andreas

  • Hi Andreas,

    I hope you are all doing well.

    I wanted to inform you that the SPI issue has been resolved. Thank you for your immersive support throughout this process.

    Below are the steps I followed to enable two SPI channels successfully:

    • Download the SDK
      https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-PvdSyIiioq/09.02.01.10/ti-processor-sdk-linux-am62xx-evm-09.02.01.10-Linux-x86-Install.bin

    • Install the SDK
      This step creates a folder named ti-processor-sdk-linux-am62xx-evm-09.02.01.09.

    • Create and Activate a Python Virtual Environment

      python3 -m venv myenv
      source myenv/bin/activate
    • Modify the Device Tree Source (DTS) File
      Change the DTS or DTSI file located at /ti-processor-sdk-linux-am62xx-evm-09.02.01.09/board-support/ti-linux-kernel-6.1.80+gitAUTOINC+2e423244f8-ti/arch/arm64/boot/dts/ti.

    • Update k3-am62x-sk-common.dtsi File
      Open k3-am62x-sk-common.dtsi and add the following lines:

        / {
            aliases {
                serial0 = &mcu_uart0;
                serial1 = &wkup_uart0;
                serial2 = &main_uart0;
                mmc0 = &sdhci0;
                mmc1 = &sdhci1;
                mmc2 = &sdhci2;
                spi0 = &ospi0;
      +         main_spi0 = &main_spi0;
      +         main_spi2 = &main_spi2;
                ethernet0 = &cpsw_port1;
                ethernet1 = &cpsw_port2;
                usb0 = &usb0;
                usb1 = &usb1;
            };
       
      +     &main_pmx0 {
      +         // SPI0
      +         main_spi0_pins_default: main-spi0-pins-default {
      +             pinctrl-single,pins = <
      +                 AM62X_IOPAD(0x01bc, PIN_INPUT, 0) /* (A14) SPI0_CLK */
      +                 AM62X_IOPAD(0x01c0, PIN_OUTPUT, 0) /* (B13) SPI0_D0 */
      +                 AM62X_IOPAD(0x01c4, PIN_INPUT, 0) /* (B14) SPI0_D1 */
      +                 AM62X_IOPAD(0x01b4, PIN_OUTPUT, 0) /* (A13) SPI0_CS0 */
      +             >;
      +         };
      + 
      +         // SPI2
      +         main_spi2_pins_default: main_spi2-pins-default {
      +             pinctrl-single,pins = <
      +                 AM62X_IOPAD(0x01b0, PIN_INPUT, 1) /* (A20) MCASP0_ACLKR.SPI2_CLK */
      +                 AM62X_IOPAD(0x0194, PIN_OUTPUT, 1) /* (B19) MCASP0_AXR3.SPI2_D0 */
      +                 AM62X_IOPAD(0x0198, PIN_INPUT, 1) /* (A19) MCASP0_AXR2.SPI2_D1 */
      +                 AM62X_IOPAD(0x01ac, PIN_OUTPUT, 7) /* (E19) MCASP0_AFSR.GPIO1_13 */
      +             >;
      +         };
      +     };
      + 
      +     &main_spi0 {
      +         status = "okay";
      +         #address-cells = <1>;
      +         #size-cells = <0>;
      +         pinctrl-names = "default";
      +         pinctrl-0 = <&main_spi0_pins_default>;
      +         ti,pindir-d0-out-d1-in;
      +         spidev@0 {
      +             spi-max-frequency = <1000000>; /* 1 MHz */
      +             reg = <0>;
      +             compatible = "rohm,dh2228fv";
      +         };
      +     };
      + 
      +     &main_spi2 {
      +         status = "okay";
      +         #address-cells = <1>;
      +         #size-cells = <0>;
      +         pinctrl-names = "default";
      +         pinctrl-0 = <&main_spi2_pins_default>;
      +         ti,pindir-d0-out-d1-in;
      +         spidev@0 {
      +             spi-max-frequency = <1000000>; /* 1 MHz */
      +             reg = <0>;
      +             compatible = "rohm,dh2228fv";
      +         };
      +     };
      + };
      

    • Update the Kernel on the SD Card

      • Get the flashed SD card and rename the ti folder in rootfs>boot to ti_old:

        sudo mv /path/to/rootfs/boot/ti /path/to/rootfs/boot/ti_old
      • Build and install the kernel:

        Use following commands to make kernel
        cd <SDK_INSTALL_DIR>/
        make linux
        sudo DESTDIR=<sdcard-mounting-point(to rootfs)> make linux_install
      • Copy the new DTB files to the ti_old folder:

        cd /path/to/rootfs/boot/ti
        sudo cp * /path/to/rootfs/boot/ti_old
      • Remove the old ti folder and rename ti_old to ti:

        sudo rm -r /path/to/rootfs/boot/ti
        sudo mv /path/to/rootfs/boot/ti_old /path/to/rootfs/boot/ti
    • Use the SD Card Normally

    Note:-

    Make sure , Before use SPI2 set following buffers 

    line   5: "EXP_PS_3V3_En" unused input active-high 

    line  10: "UART1_FET_BUF_EN" unused input active-high 

    line  21: "UART1_FET_SEL" unused input active-high 

    Run following in the command line to set above buffers

    gpioset  gpiochip2  5=1 

    gpioset  gpiochip2  10=1 

    gpioset  gpiochip2  21=0 

     

    With these steps, I was able to enable and test the two SPI channels successfully.

    Thank you again for your support.

    Best regards,

    Kasun

  • Hi Kasun,

    thank you for sharing the steps; I'm sure it'll be helpful to somebody else!!

    Regards, Andreas