This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B-P1: Issue with USB Host Mode Data Transfer and Support Query

Hi,

We tested the USB host mode functionality using the lsusb library. While the application shows that data is being sent, we are unable to access the data on a USB device when connected to a personal PC for verification.

Test Summary:

  • Tested Feature: USB Host Mode
  • Tool Used: lsusb library
  • Observation: USB Host Mode is able to send data, but the sent data cannot be accessed on a personal PC when verified using a USB device.

Query:

  • Does the USB host mode support only booting, or does it also support data transfer from the device to another USB device?

Please provide guidance on resolving the data access issue and clarify the capabilities of the USB host mode regarding booting and data transfer.

Regards,Vikash