Tool/software:
Dear TI Expert,
1. Target Product
- TDA4VE on J721S2
2. Questionnaire
- As per the lockstep core, which is activated on R5F Core on MCU Domain, the lockstep testing is only executed during boot phase ?
- If so, Application SW can be loaded after the phase ?
3. Background
- I am an Automotive engineer, and we will apply lockstep on the core so that required ASIL is satisfied as per the requirement
- BTW, once the lockstep is activated, we might lose one extra core which is able to load an application SW,
- so if there is a guidance which can execute the lockstep only in boot phase and run a application SW during the runtime, please share us