This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi all,
we are trying to configure usb0 to work as host so that when we connect a device like usb it will read the data from the usb.
our hardware connections are made in a way that Vbus, cc1 and CC2 are connected to the +5v. Usb id is connected to 1v8.
Rest of the connections are USB_1_D_CON_P and USB_1_D_CON_N are connected to the USB-c connector.
below are the device tree configurations:
/* Verdin USB_1_ID */ pinctrl_usb0_id: main-gpio1-19-pins-default { pinctrl-single,pins = < AM62X_IOPAD(0x01c4, PIN_INPUT_PULLUP, 7) /* (B14) SPI0_D1.GPIO1_19 */ /* SODIMM 161 */ >; }; /* Verdin USB_1 */ &usbss0 { ti,vbus-divider; status = "okay"; connector { compatible = "gpio-usb-b-connector", "usb-b-connector"; pinctrl-names = "default"; pinctrl-0 = <>; label = "USB-C"; port { usb_dr_connector: endpoint { remote-endpoint = <&usb0_ep>; }; }; }; }; &usb0 { dr_mode = "host"; status="okay"; port { usb0_ep: endpoint { remote-endpoint = <&usb_dr_connector>; }; }; };
kindly check this and let me know if i am doing something wrong
Hi,
Thanks for your reply.
currently below is my device tree changes:
/* Verdin USB_1 */ &usbss0 { ti,vbus-divider; status = "okay"; debounce = <25>; id-gpio = < >; pinctrl-names = "default"; }; &usb0 { dr_mode = "host"; status="okay"; };
we are using a type-c port for connecting devices like usb storage devices. as mentioned above vbus, cc1 and cc2 are connected to the 5v and id is connected to the gnd. and drvvbus is not connected.
Hi,
The "debounce" and "id-gpio" properties should be removed from &usbss0 node.
The ID pin is not needed.
When dr_mode is et to "host", the USB controller doesn't communicate with the type-C device for role switching, so the CC pins should be connected based on the type-C device requirement (which I am not familiar with though).
If the USB drvvbus pin is not connected, the VBUS 5v power switch should be controlled by something else (the type-C device?).
Do we need usb controller ic in this case ? If we use the type c ?
Currently vbus is just directly connected to 5v!
Any suggestions on how to usually make a usb type c to work as host
Thanks in advance
Hi,
Do we need usb controller ic in this case ? If we use the type c ?
That is a good question. From the software perspective, the type-C IC is not needed if the USB controller works in host-only mode. However, the USB type-C receptacle has two sets of DP/DM pins, without a type-C IC, both sets of DP/DM would have to be routed together to the DP/DM pins of the AM62x USB0 port, I am a software buy, but I believe this 'Y' type USB signal routing is not allowed, it could cause USB signal integrity problem. I am looping in our USB hardware expert to comment on this.
Hello Naveen,
You might want to refer to the different implementations we have on the SKs.
Please review below
Recommended References for review and design of custom board
AM62X
Hardware Design Considerations
www.ti.com/.../sprad05b.pdf
Schematic Design and Review Checklist
www.ti.com/.../sprad21c.pdf
DDR Board Design and Layout Guidelines
www.ti.com/.../sprad06.pdf
Frequently Asked Questions FAQs
e2e.ti.com/.../faq-custom-board-hardware-design---master-complete-list-of-faqs-for-all-sitara-processor-am62x-am64x-am243x-am335x-families
e2e.ti.com/.../faq-am625-am623-am625sip-am625-q1-am620-q1-custom-board-hardware-design---faqs-related-to-processor-collaterals-functioning-peripherals-interface-and-starter-kit
e2e.ti.com/.../faq-am625-am623-custom-board-hardware-design---design-and-review-notes-for-reuse-of-sk-am62b-schematics
e2e.ti.com/.../faq-am625-am623-custom-board-hardware-design---design-and-review-notes-for-reuse-of-sk-am62b-p1-schematics
e2e.ti.com/.../faq-am625-q1-am620-q1-custom-board-hardware-design---design-and-review-notes-for-reuse-of-sk-am62-lp-schematics
e2e.ti.com/.../faq-am625sip---custom-board-hardware-design---design-and-review-notes-for-reuse-of-sk-am62-sip-schematics
e2e.ti.com/.../faq-am62x-am64x-custom-board-hardware-design-how-to-handle-used-unused-pins-peripherals-e-g-gpios-serdes-usb-csi-mmc-emmc-sd-card-csi-oldi-dsi
Downloadable design files on TI.com list for SK
SK-AM62B-P1 Design Package Content Overview (Rev. A)
www.ti.com/.../sprt777
SK-AM62-LP Design Package Content Overview
www.ti.com/.../sprt778
SK-AM62B Design Package Folder and Files List
www.ti.com/.../sprt784
SK-AM62-SIP Design Package Folder and Files List
https://www.ti.com/lit/pdf/sprt785
Regards,
Sreenivasa
HI all,
Thanks all for your valuable inputs. I have shared everything to our hardware team. Below is the USB schematic configuration in our board.
In this few changes were made recently were, VbUS is connected to +5V and CC1 And CC2 and also connected to +5v. It is a usb type-c port.
Hi,
I guess I should have asked the question in the very beginning - are you looking for comments in your board USB design schematics, or your board USB doesn't work as expected and need debug?
have you measured the VBUS pin on the USB-C connector that the 5V presents when attaching a USB device?
Please run the following script on your board and provide its output.
#!/bin/bash # # Util to check USB subsystem for Linux kernel 4.0+ on TI Sitara devices # # Copyright (C) 2018-2024 Texas Instruments Incorporated - http://www.ti.com/ # # # Redistribution and use in source and binary forms, with or without # modification, are permitted provided that the following conditions # are met: # # Redistributions of source code must retain the above copyright # notice, this list of conditions and the following disclaimer. # # Redistributions in binary form must reproduce the above copyright # notice, this list of conditions and the following disclaimer in the # documentation and/or other materials provided with the # distribution. # # Neither the name of Texas Instruments Incorporated nor the names of # its contributors may be used to endorse or promote products derived # from this software without specific prior written permission. # # THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS # "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT # LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR # A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT # OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, # SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT # LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, # DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY # THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT # (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE # OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. VERSION=0.4.0 DTPATH=/sys/firmware/devicetree/base DEVPATH=/sys/devices/platform KMODPATH="/lib/modules/`uname -r`" ### ENV # $V: debug flag # $PLATFORM: force g_plaform if not found in device tree ### functions ### # $1 commands to be checked check_command() { local _lst="$*" local _cmd for _cmd in $_lst; do which $_cmd > /dev/null || { echo "Error: $_cmd command not found" exit 1 } done } # check if the kernel is supported # this tool only runs on v4.0+ kernel # return 0 - if kernel version >= 4.0 # 1 - if kernel version < 4.0 has_supported_kernel() { local _ver local _t check_command uname uname -a _ver=`uname -r` _t=${_ver%%.*} # 3.x.x or older, unsupported [ $_t -ge 4 ] || return 1 return 0 } # define variables for musb entries in sysfs and device tree # output variables: USB_DT_PARENT, USB0DT, USB1DT # USB_DEV_PARENT, USB0DEV, USB1DEV query_musb_entries() { local _lst local _t local _intr check_command find # find usb entry names in device-tree _t=$(find ${DTPATH}/ -maxdepth 2 -name '*47400000*') [ -n "$_t" ] && USB_DT_PARENT=$_t || { echo "usb parent DT node not found in device-tree" exit 1 } _lst=$(find ${USB_DT_PARENT}/ -maxdepth 1 -name 'usb@*') [ -n "$_lst" ] || { echo "usb0 and usb1 DT node not found in device-tree" exit 1 } # find USB child DT node based on its interrupt number for _t in $_lst; do [[ -f "${_t}/interrupts" ]] || continue _intr=$(hexdump ${_t}/interrupts | head -1 | cut -d' ' -f3) case $_intr in "1200") USB0DT=$_t;; "1300") USB1DT=$_t;; *) echo "unkown usb interrupt number $_intr" exit 1 esac done # find device names in sysfs _t=$(find ${DEVPATH}/ -maxdepth 2 -name '*47400000*') [ -n "$_t" ] && USB_DEV_PARENT=$_t || { echo "usb device not found in sysfs" exit 1 } _t=$(find ${USB_DEV_PARENT}/47401400.usb/ -maxdepth 1 -name 'musb-hdrc.*') [ -n "$_t" ] && USB0DEV=$_t || echo "usb0 device not found in sysfs" _t=$(find ${USB_DEV_PARENT}/47401c00.usb/ -maxdepth 1 -name 'musb-hdrc.*') [ -n "$_t" ] && USB1DEV=$_t || echo "usb1 device not found in sysfs" } # check if the platform is supported # return 0 - if platform is supported # 1 - if platform is not supported check_platform () { local _hw check_command grep _hw=`cat ${DTPATH}/compatible | tr '\0' ' '` DBG_PRINT "DT compatible: $_hw" if [[ "$_hw" == *"ti,am33xx"* ]]; then g_platform="am335x" elif [[ "$_hw" == *"ti,am43"* ]]; then g_platform="am437x" elif [[ "$_hw" == *"ti,am62"* ]]; then g_platform="am62xx" else # read from ENV g_platform=$PLATFORM fi DBG_PRINT "g_platform: $g_platform" case $g_platform in "am335x") query_musb_entries return 0;; "am437x") USB0DT="$(find $DTPATH -name 'usb@48390000')" USB1DT="$(find $DTPATH -name 'usb@483d0000')" return 0;; "am62xx") USB0DT="$(find $DTPATH -name 'usb@31000000')" USB1DT="$(find $DTPATH -name 'usb@31100000')" return 0;; *) echo "Unsupported \"$g_platform\"" return 1;; esac } # get kernel config options from /proc/config.gz # params $@ - the list of config options to query, without 'CONFIG_' # return - the config options settings in /proc/config.gz get_kernel_configs() { local _opts="$@" local _lst="" local _t check_command zcat grep for _t in $_opts; do [ -z "$_lst" ] && _lst="^CONFIG_${_t}\>" || _lst="${_lst}\|^CONFIG_${_t}\>" done [ -z "$_lst" ] || zcat /proc/config.gz | grep "$_lst" } # check a kernel CONFIG option # params $1 - the config option list returned from get_kernel_config() # if "", directly check $2 from /proc/config.gz # $2 - the config option to check # $3 = '-q', quiet output # return 0 - undefined # 1 - defined as 'm', kernel module # 2 - defined as 'y', kernel builtin check_kernel_config() { local _cfg local _t [ -n "$2" ] || return 0 if [ -z "$1" ]; then check_command zcat _cfg=`zcat /proc/config.gz | grep "^$2\>"` else for _t in $1; do [[ "$_t" != "${2}="? ]] || { _cfg=$_t; break; } done fi case ${_cfg#*=} in "y") return 2;; "m") return 1;; *) [ "$3" = "-q" ] || echo "Error: $2 is undefined in kernel config" return 0;; esac } # check a kernel module # $1 - module name, relative path from drivers/, without .ko surfix # return 0 - found # 1 - error check_module() { local _modname local _moddep [ -n "$1" ] || return 1 _modname="${KMODPATH}/kernel/drivers/${1}.ko" _moddep="${KMODPATH}/modules.dep" DBG_PRINT "${1}.ko checking..." [ -f $_modname ] || { echo "Error: $_modname not found." echo " Please ensure 'make module_install' is done properly." return 1 } DBG_PRINT "${1}.ko found" [ -f $_moddep ] || $g_printed_once || { echo "Error: $_moddep not found." echo " Please ensure 'make module_install' is done properly." g_printed_once=true } DBG_PRINT "${1}.ko moddep checked" check_command lsmod basename tr lsmod | grep `basename $1 | tr '-' '_'` > /dev/null || { DBG_PRINT ">>>> ${1}.ko not found in lsmod:" if grep "${1}.ko:" $_moddep > /dev/null; then echo "Error: $_moddep seems to be valid," echo " but `basename $1`.ko is not loaded." echo " Please provide /proc/config.gz and ${KMODPATH}/*" echo " for further investigation." else echo "Error: `basename $1`: $_moddep is invalid." echo " Please run command 'depmod' on the target to re-generate it," echo " then reboot the target. If the issue still exists, please" echo " ensure 'make module_install' is done properly." fi return 1 } DBG_PRINT "${1}.ko done" return 0 } # check kernel config, and modules (if CONFIG_*=M) for musb check_musb_drivers() { local _lst=("USB_MUSB_HDRC" "USB_MUSB_DUAL_ROLE" "USB_OTG" "USB_MUSB_DSPS" \ "AM335X_PHY_USB" "MUSB_PIO_ONLY" "TI_CPPI41") local _opts _opts=$(get_kernel_configs ${_lst[*]}) check_kernel_config "$_opts" CONFIG_USB_MUSB_HDRC [ $? != 1 ] || check_module 'usb/musb/musb_hdrc' check_kernel_config "$_opts" CONFIG_USB_MUSB_DUAL_ROLE -q [ $? != 0 ] || echo "Warning: CONFIG_USB_MUSB_DUAL_ROLE undefined." check_kernel_config "$_opts" CONFIG_USB_OTG -q [ $? == 0 ] || echo "Warning: CONFIG_USB_OTG defined." check_kernel_config "$_opts" CONFIG_USB_MUSB_DSPS [ $? != 1 ] || { check_module 'usb/musb/musb_dsps' } check_kernel_config "$_opts" CONFIG_AM335X_PHY_USB [ $? != 1 ] || { check_module 'usb/phy/phy-am335x' check_module 'usb/phy/phy-am335x-control' } check_kernel_config "$_opts" CONFIG_MUSB_PIO_ONLY -q [ $? != 0 ] || { if check_kernel_config "$_opts" CONFIG_TI_CPPI41 -q; then echo "Error: MUSB CPPI DMA mode is enabled, but CPPI moudle is not enabled in DMA Engine." echo " Please enable CONFIG_TI_CPPI41 under DMA Engine Support in kernel config." fi } } # check kernel config, and modules (if CONFIG_*=M) for am437x dwc3 check_dwc3_am437x_drivers() { local _lst=("USB_DWC3" "USB_DWC3_DUAL_ROLE" "USB_OTG" "USB_DWC3_OMAP" \ "USB_XHCI_HCD" "OMAP_CONTROL_PHY" "OMAP_USB2") local _opts _opts=$(get_kernel_configs ${_lst[*]}) check_kernel_config "$_opts" CONFIG_USB_DWC3 [ $? != 1 ] || check_module 'usb/dwc3/dwc3' check_kernel_config "$_opts" CONFIG_USB_DWC3_DUAL_ROLE -q [ $? != 0 ] || echo "Warning: CONFIG_USB_DWC3_DUAL_ROLE undefined." check_kernel_config "$_opts" CONFIG_USB_OTG -q [ $? == 0 ] || echo "Warning: CONFIG_USB_OTG defined." check_kernel_config "$_opts" CONFIG_USB_DWC3_OMAP [ $? != 1 ] || check_module 'usb/dwc3/dwc3-omap' check_kernel_config "$_opts" CONFIG_USB_XHCI_HCD [ $? != 1 ] || { check_module 'usb/host/xhci-plat-hcd' check_module 'usb/host/xhci-hcd' } check_kernel_config "$_opts" CONFIG_OMAP_CONTROL_PHY [ $? != 1 ] || check_module 'phy/phy-omap-control' check_kernel_config "$_opts" CONFIG_OMAP_USB2 [ $? != 1 ] || check_module 'phy/phy-omap-usb2' } # check kernel config, and modules (if CONFIG_*=M) for am62xx dwc3 check_dwc3_am62xx_drivers() { local _lst=("USB_DWC3" "USB_DWC3_DUAL_ROLE" "USB_DWC3_AM62" \ "USB_XHCI_HCD") local _opts _opts=$(get_kernel_configs ${_lst[*]}) check_kernel_config "$_opts" CONFIG_USB_DWC3 [ $? != 1 ] || check_module 'usb/dwc3/dwc3' check_kernel_config "$_opts" CONFIG_USB_DWC3_DUAL_ROLE -q [ $? != 0 ] || echo "Warning: CONFIG_USB_DWC3_DUAL_ROLE undefined." check_kernel_config "$_opts" CONFIG_USB_DWC3_AM62 [ $? != 1 ] || check_module 'usb/dwc3/dwc3-am62' check_kernel_config "$_opts" CONFIG_USB_XHCI_HCD [ $? != 1 ] || { check_module 'usb/host/xhci-plat-hcd' check_module 'usb/host/xhci-hcd' } } check_musb_dt() { local _dt_dir local _ent local _sts local _t case $USB_DT_PARENT in *"usb@"*) _ent=("control@44e10620" "usb-phy@47401300" "usb-phy@47401b00" \ "usb@47401000" "usb@47401800" "dma-controller@47402000") ;; *"target-module@"*) _ent=("usb-phy@1300" "usb-phy@1b00" "usb@1400" "usb@1800" \ "dma-controller@2000") ;; *) echo "Warning: unknown USB DT ($USB_DT_PARENT)" return esac echo "Device Tree USB node status:" for _t in '.' ${_ent[*]}; do [ -d "${USB_DT_PARENT}/${_t}/" ] || { echo -e "\tWarning: USB DT node $_t not found" continue } [ -f "${USB_DT_PARENT}/${_t}/status" ] && _sts=$(tr -d '\0' <${USB_DT_PARENT}/${_t}/status) || _sts="(enabled)" echo -e "\t$_t: $_sts" done } dump_sysfs_debugfs() { local _debugfs local _l local _f _debugfs=`sed -ne 's/^debugfs \(.*\) debugfs.*/\1/p' /proc/mounts` [ -n "$_debugfs" ] || return case $g_platform in am335x) _debugfs=$(find $_debugfs -name 'musb-hdrc.*') _debugfs=${_debugfs%/*} for _f in $USB0DEV $USB1DEV; do _l=$(basename $_f) echo "$_l: mode $(cat ${_f}/mode), $(cat ${_f}/vbus)" grep -i 'power\|devctl\|testmode' ${_debugfs}/${_l}/regdump done ;; esac } check_gadget_kernel_config() { local _lst=("USB_ZERO" "USB_AUDIO" "USB_ETH" "USB_G_NCM" "USB_MASS_STORAGE" \ "USB_G_SERIAL" "USB_G_PRINTER") local _opts _opts=$(get_kernel_configs ${_lst[*]}) check_kernel_config "$_opts" CONFIG_USB_ZERO -q || echo "Gadget Kernel Config: g_zero is enabled" check_kernel_config "$_opts" CONFIG_USB_AUDIO -q || echo "Gadget Kernel Config: g_audio is enabled" check_kernel_config "$_opts" CONFIG_USB_ETH -q || echo "Gadget Kernel Config: g_ether is enabled" check_kernel_config "$_opts" CONFIG_USB_G_NCM -q || echo "Gadget Kernel Config: g_ncm is enabled" check_kernel_config "$_opts" CONFIG_USB_MASS_STORAGE -q || echo "Gadget Kernel Config: g_mass_storage is enabled" check_kernel_config "$_opts" CONFIG_USB_G_SERIAL -q || echo "Gadget Kernel Config: g_serial is enabled" check_kernel_config "$_opts" CONFIG_USB_G_PRINTER -q || echo "Gadget Kernel Config: g_printer is enabled" } ### debug ### g_log_file=/tmp/chkusb.log DBG_ENABLE() { g_dbg_enabled=true; } DBG_DISABLE() { g_dbg_enabled=false; } DBG_LOG_RESET() { ! $g_dbg_enabled || echo > $g_log_file; } DBG_PRINT() { ! $g_dbg_enabled || echo "$(date +%H:%M:%S) [$(basename $0)]: $*"; } DBG_LOG() { DBG_PRINT $* >> $g_log_file; } DBG_LOG_MARK() { DBG_PRINT "----------------" >> $g_log_file; } ### main #### g_printed_once=false echo "chkusb.sh Version $VERSION" [ "$V" = "1" ] && DBG_ENABLE && DBG_LOG_RESET || DBG_DISABLE has_supported_kernel || { echo "Unsupported kernel version: `uname -r`"; exit 1; } check_platform || exit 2 DBG_PRINT device: $g_platform [ -d ${DTPATH} ] || { echo "Error: ${DTPATH} not found"; exit 3; } check_command lsusb if lsusb > /dev/null 2>&1; then echo "USB is initialized" else echo "USB initialization failed" fi # check kernel configs if [ -f /proc/config.gz ]; then case $g_platform in am335x) check_musb_drivers;; am437x) check_dwc3_am437x_drivers;; am62xx) check_dwc3_am62xx_drivers;; esac else echo "Error: /proc/config.gz not found" fi dump_sysfs_debugfs # check dr_mode & gadget drivers check_command basename for _usb_dir in "${USB0DT}" "${USB1DT}"; do [ -n "$_usb_dir" ] || continue [ -f "$_usb_dir/status" ] && _status=`tr -d '\0' <$_usb_dir/status` || _status='(enabled)' _dr_mode=`tr -d '\0' <$_usb_dir/dr_mode` echo `basename $_usb_dir`: $_dr_mode, $_status [ "$_status" = "disabled" -o "$_dr_mode" = "host" ] || gadget_mode=true done case $g_platform in am335x) check_musb_dt;; *) ;; esac DBG_PRINT $gadget_mode $gadget_mode || exit 0 echo check_kernel_config "" CONFIG_USB_LIBCOMPOSITE case $? in 0) echo "Error: no any gadget driver enabled" exit 6;; 1) is_gadget_builtin=false;; 2) echo "The gadget driver is built-in" is_gadget_builtin=true;; esac [[ ! -f /proc/config.gz ]] || check_gadget_kernel_config g_driver=`grep '^DRIVER=' /sys/class/udc/*/uevent 2>/dev/null` echo "gadget driver loaded: ${g_driver:-(none)}" [[ $is_gadget_builtin == false ]] || exit 0 echo if [ -d "$KMODPATH" ]; then echo "The list of USB gadget drivers installed:" ls -1Rp ${KMODPATH}/kernel/drivers/usb/gadget/{function,legacy}/ else echo "Error: $KMODPATH not found" echo " Please ensure 'make modules_install' is done properly." exit 7 fi # vim: ft=sh:ts=4:sw=4:et
Hi bin liu,
please find the output below,
chkusb.sh Version 0.4.0 Linux verdin-am62-15133535 6.1.80-6.7.0-devel+git.603f75dc931d #1 SMP PREEMPT Wed Aug 28 15:15:41 UTC 2024 aarch64 aarch64 aarch64 GNU/Linux USB is initialized usb@31000000: host, okay usb@31100000: otg, (enabled) Gadget Kernel Config: g_zero is enabled Gadget Kernel Config: g_ether is enabled Gadget Kernel Config: g_ncm is enabled Gadget Kernel Config: g_mass_storage is enabled Gadget Kernel Config: g_serial is enabled gadget driver loaded: (none) The list of USB gadget drivers installed: /lib/modules/6.1.80-6.7.0-devel+git.603f75dc931d/kernel/drivers/usb/gadget/function/: u_ether.ko u_serial.ko usb_f_acm.ko usb_f_ecm.ko usb_f_ecm_subset.ko usb_f_eem.ko usb_f_fs.ko usb_f_mass_storage.ko usb_f_ncm.ko usb_f_obex.ko usb_f_rndis.ko usb_f_serial.ko usb_f_ss_lb.ko /lib/modules/6.1.80-6.7.0-devel+git.603f75dc931d/kernel/drivers/usb/gadget/legacy/: g_cdc.ko g_ether.ko g_mass_storage.ko g_multi.ko g_ncm.ko g_serial.ko g_zero.ko gadgetfs.ko
Currently Vbus is connected to a 5V using pullup resistor, it always stays at 5V
Hi,
The log seems indicating the USB controller is in the correct state.
Please use a scope to capture the waveform of DP/DM and VBUS lines when a USB device is attached.
Hi,
If DP or DM line doesn't pullup when the USB device is attached, mostly likely the device doesn't get 5V on VBUS. Please check on the type-C connector that 5V does present.
we are able to see DP and DM pulling up to 3.3v and vbus is also 5v.but still the device is not detected. anything else we can check.
What change have you made to make you see DP and DM pullup now? Please attach the scope screenshot.
Does the board Linux console print any message when the USB device attached? If so, please attach the console log.
Please attach the scope screenshot to show the waveform of DP/DM pulling up along with VBUS line when the USB device is attached.
Please set the scope horizontal resolution to millisecond resolution, and compare the waveform with a working USB host.
I believe, when you attach a high-speed USB device, it should only have DP get pulled up, DM should stay low. But I don't know why you see both DP and DM get pulled up.
Hi bin liu,
Thanks for your help, we are able make usb work,
below is the device tree:
/* Verdin USB_1 */
&usbss0 {
ti,vbus-divider;
status="okay";
};
&usb0 {
dr_mode = "host";
status = "okay";
}
The issue is that, the transformer used on the DP/DM was placed wrongly, now we have corrected at it worked.