Part Number: AM625
Other Parts Discussed in Thread: SK-AM62
Tool/software:
Hi,
I have a custom board based on SK-AM62. Based on the console output(attached below), it seems DDR4 is not initialized and booting stop there. I have followed the thread below which had similar issue for AM64x device.
I applied the patch file given in the thread. But I dont see any DDR4 traning happening. Console output stil remains same as below.
U-Boot SPL 2021.01-00001-ga347ec164e-dirty (May 07 2024 - 13:33:51 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13384 bytes
Please find the schematic attached for your reference. I have probed DDR_RESET and CKE signal and that looks fine too. Please give me a guidance to debug this issue. Also, I have a question that, this patch is generic for all am6xx device or only AM64x device?



Thanks,
siva.