Tool/software:
Hi team,
It is my and the customer's understanding that they can utilize the SERDES REFCLK as an output on the AM6422 due to the updates in the errata. However, other than showing the signal pair as I/O in various tables and figures, there is nothing that talks about using SERDES REFCLK as an output in the datasheet or TRM. Datasheet section 6.10.4.1, Input Clocks / Oscillators, calls it an optional reference clock input for PCIe and 6.10.4.2, Output Clocks, does not mention it.
Where is SERDES0_REFCLK0 used as an output discussed other than the errata? Sourcing the PCIe reference clock from the CPU and providing to the FPGA would be desirable for them.
Is an output clock the default setting for the SERDES REFCLK? Does anything need to be programmed to generate the output clock? What is inside the device and what does the PWB need to provide (series resistors, resistors to ground)?
Thanks,
Luke