Dear Ti Team,
We are facing one issue related USB mass storage module.
we are inserting g_mass_storage.ko module and mounting one sd-card on the Host PC.
When we run the crystal disk mark utility to test the write performance, we are getting the below
mentioned prints on the board because of which we are getting write performance very low.
g_mass_storage gadget: high speed config #1: Linux File-Backed Storage.
Then we run the USB Analyzer on the host PC and found out that sometimes when 64k data is transfered,
board is not giving response back because of which host PC is Resetting the USB Port. Please find the log below.
We are using the Kernel from PSP=v2.6.37_ti816xpsp_04.00.02.14 release.
Please let us know the solution for this as soon as possible.
Best Regards,
Supreet