This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Strange SRIO response packet.



Hello. I'm sending Message Type 11 packets from FPGA to C6678 DSP using SRIO. DSP is sending strange responses like this: Ftype = 0x0D, Ttype = 0x01, Status Field = 0x07 (Error), Transaction ID always = 50 (on DSP SYS-BIOS 6 is running, and SRIO type-11 socket is opened). When I send from FPGA NWRITE_R operation, it works fine, and Responses received from DSP are alright: transaction ID increments normally and matches transaction ID of request-message, Status = 0 (DONE), Ttype = 0x00, Ftype = 0x0D.

What is strange Transaction ID (50) in message-response packets and why this error occurs?