This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi all,
i have to interface two LPDDR SDRAM to SDRC of OMAP 3530. each chip select can support 512 MB SDRAM.
if we interface two 1 GB LPDDR SDRAM to SDRC instead of 512 MB, does it create any problem ..?
thanks and regards
N reddy
Max per chip select is 512 MB. Total memory across CS0 and CS1 is a max of 1 GB.
regards,
Michael