Part Number: AM2634
Other Parts Discussed in Thread: LP-XDS110
Hello,
I am trying to connect to an AM2634 on my custom PCB for debugging using an external LP-XDS110 Debugger. CCS reports a DAP access error when I start debugging. The full message text is:
CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation.
If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 21.0.0.3955) .
My development setup is as follows:
-MCU part number is AM2634CODFHAZCZR.
-CCS version is 21.0.0.
- I am using LP-XDS110 Debugger to connect to the chip. Debugger is connected through TCK, TMS, TDI, TDO and GND. 3.3V output is not currently connected
Initially, the switches in the SOP selection circuit were configured for DevBoot according to the table shown below. I then tried the inverse configuration, because I was unsure whether the table indicated the switches’ open/closed states or the actual HIGH/LOW logic levels at the MCU’s SOP pins. Nonetheless, CCS reported the same DAP access error in both cases.
I have attached the SOP selection schematic and the boot-mode table below for reference. The pull-up and DNP resistor settings in the schematic were also changed and made compliant to DevBoot configuration.
I would also appreciate clarification on the table issue.